hidkbd.c File Reference

USB Human Interface Devices (HID) class keyboard driver.

Version
5.6.0

License

Copyright 2015 Silicon Labs, Inc. http://www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file hidkbd.c .

#include " em_device.h "
#include " em_common.h "
#include "em_usb.h"
#include " hidkbd.h "

Macros

#define DEFAULT_IDLE_RATE 500

Functions

void HIDKBD_Init ( HIDKBD_Init_t *init)
Initialize HID Keyboard driver.
void HIDKBD_KeyboardEvent ( HIDKBD_KeyReport_t *report)
Report a keyboard press/release event.
int HIDKBD_SetupCmd (const USB_Setup_TypeDef *setup)
Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.
void HIDKBD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState)
Handle USB state change events, this function must be called each time the USB device state is changed.
const char HIDKBD_ReportDescriptor[69] SL_ATTRIBUTE_ALIGN (4)

Macro Definition Documentation

#define DEFAULT_IDLE_RATE   500

Default idle-rate recommended in the USB HID class specification.

Definition at line 61 of file hidkbd.c .

Referenced by HIDKBD_StateChangeEvent() .

Function Documentation

const char HIDKBD_ReportDescriptor [69] SL_ATTRIBUTE_ALIGN ( 4 )

HID report descriptor created with usb.org's "HID Descriptor Tool(DT)" version 2.4. The descriptor defines an input report which matches the HIDKBD_KeyReport_t typedef, and an output report with 3 bits for controlling NumLock, CapsLock and ScrollLock keyboard LED's