dmadrv.c File Reference
DMADRV API implementation.
- Version
- 5.6.0
License
(C) Copyright 2014 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        dmadrv.c
       
       .
      
       #include <stdbool.h>
      
      
       #include <stddef.h>
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_cmu.h
       
       "
      
      
       #include "
       
        em_core.h
       
       "
      
      
       #include "
       
        dmadrv.h
       
       "
      
      
| Functions | |
| Ecode_t | DMADRV_AllocateChannel (unsigned int *channelId, void *capabilities) | 
| Allocate (reserve) a DMA channel. | |
| Ecode_t | DMADRV_DeInit (void) | 
| Deinitialize DMADRV. | |
| Ecode_t | DMADRV_FreeChannel (unsigned int channelId) | 
| Free an allocated (reserved) DMA channel. | |
| Ecode_t | DMADRV_Init (void) | 
| Initialize DMADRV. | |
| Ecode_t | DMADRV_LdmaStartTransfer (int channelId, LDMA_TransferCfg_t *transfer, LDMA_Descriptor_t *descriptor, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start an LDMA transfer. | |
| Ecode_t | DMADRV_MemoryPeripheral (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src, bool srcInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start a memory to a peripheral DMA transfer. | |
| Ecode_t | DMADRV_MemoryPeripheralPingPong (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src0, void *src1, bool srcInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start a memory to a peripheral ping-pong DMA transfer. | |
| Ecode_t | DMADRV_PauseTransfer (unsigned int channelId) | 
| Pause an ongoing DMA transfer. | |
| Ecode_t | DMADRV_PeripheralMemory (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src, bool dstInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start a peripheral to memory DMA transfer. | |
| Ecode_t | DMADRV_PeripheralMemoryPingPong (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst0, void *dst1, void *src, bool dstInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start a peripheral to memory ping-pong DMA transfer. | |
| Ecode_t | DMADRV_ResumeTransfer (unsigned int channelId) | 
| Resume an ongoing DMA transfer. | |
| Ecode_t | DMADRV_StopTransfer (unsigned int channelId) | 
| Stop an ongoing DMA transfer. | |
| Ecode_t | DMADRV_TransferActive (unsigned int channelId, bool *active) | 
| Check if a transfer is running. | |
| Ecode_t | DMADRV_TransferCompletePending (unsigned int channelId, bool *pending) | 
| Check if a transfer complete is pending. | |
| Ecode_t | DMADRV_TransferDone (unsigned int channelId, bool *done) | 
| Check if a transfer has completed. | |
| Ecode_t | DMADRV_TransferRemainingCount (unsigned int channelId, int *remaining) | 
| Get number of items remaining in a transfer. | |