RMUEMLIB
Detailed Description
Reset Management Unit (RMU) Peripheral API.
This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.
| Macros | |
| #define | RMU_LockupResetDisable (A) RMU_ResetControl ( rmuResetLockUp , A) | 
| Enumerations | |
| enum | RMU_Reset_TypeDef
         
         { rmuResetLockUp = _RMU_CTRL_LOCKUPRMODE_MASK, rmuResetWdog = _RMU_CTRL_WDOGRMODE_MASK, rmuResetCoreLockup = _RMU_CTRL_LOCKUPRMODE_MASK, rmuResetSys = _RMU_CTRL_SYSRMODE_MASK, rmuResetPin = _RMU_CTRL_PINRMODE_MASK } | 
| enum | RMU_ResetMode_TypeDef
         
         { rmuResetModeDisabled = _RMU_CTRL_PINRMODE_DISABLED, rmuResetModeLimited = _RMU_CTRL_PINRMODE_LIMITED, rmuResetModeExtended = _RMU_CTRL_PINRMODE_EXTENDED, rmuResetModeFull = _RMU_CTRL_PINRMODE_FULL } | 
| Functions | |
| void | RMU_ResetCauseClear (void) | 
| Clear the reset cause register. | |
| uint32_t | RMU_ResetCauseGet (void) | 
| Get the cause of the last reset. | |
| void | RMU_ResetControl ( RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode) | 
| Disable/enable reset for various peripherals and signal sources. | |
| __STATIC_INLINE uint32_t | RMU_UserResetStateGet (void) | 
| Get user reset state. Reset only by a Power-on-reset and a pin reset. | |
| __STATIC_INLINE void | RMU_UserResetStateSet (uint32_t userState) | 
| Set user reset state. Reset only by a Power-on-reset and a pin reset. | |
Macro Definition Documentation
| #define RMU_LockupResetDisable | ( | 
            A
            | ) | RMU_ResetControl ( rmuResetLockUp , A) | 
RMU_LockupResetDisable kept for backwards compatibility.
        Definition at line
        
         133
        
        of file
        
         em_rmu.h
        
        .
       
Enumeration Type Documentation
| enum RMU_Reset_TypeDef | 
RMU reset modes.
        Definition at line
        
         61
        
        of file
        
         em_rmu.h
        
        .
       
Function Documentation
| void RMU_ResetCauseClear | ( | void | 
            | ) | 
Clear the reset cause register.
This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet() .
        Definition at line
        
         276
        
        of file
        
         em_rmu.c
        
        .
       
References BUS_RegBitWrite() , EMU , EMU_Lock() , EMU_LOCK_LOCKKEY_LOCKED , EMU_Unlock() , RMU , and RMU_CMD_RCCLR .
Referenced by SLEEP_Init() .
| uint32_t RMU_ResetCauseGet | ( | void | 
            | ) | 
Get the cause of the last reset.
To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear() . This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".
- Returns
- A reset cause mask. See the reference manual for a description of the reset cause mask.
        Definition at line
        
         319
        
        of file
        
         em_rmu.c
        
        .
       
References EMU , EMU_BASE , RMU , RMU_RSTCAUSE_AVDDBOD , RMU_RSTCAUSE_DECBOD , RMU_RSTCAUSE_DVDDBOD , RMU_RSTCAUSE_EM4RST , RMU_RSTCAUSE_EXTRST , RMU_RSTCAUSE_LOCKUPRST , RMU_RSTCAUSE_SYSREQRST , and RMU_RSTCAUSE_WDOGRST .
Referenced by SLEEP_Init() .
| void RMU_ResetControl | ( | RMU_Reset_TypeDef | 
            reset,
            | 
| RMU_ResetMode_TypeDef | 
            mode
            | ||
| ) | 
Disable/enable reset for various peripherals and signal sources.
- Parameters
- 
         [in] resetReset types to enable/disable.s [in] modeReset mode. 
        Definition at line
        
         248
        
        of file
        
         em_rmu.c
        
        .
       
References BUS_RegBitWrite() , EMU , RMU , and SL_CTZ() .
| __STATIC_INLINE uint32_t RMU_UserResetStateGet | ( | void | 
            | ) | 
Get user reset state. Reset only by a Power-on-reset and a pin reset.
- Returns
- Reset surviving user state.
        Definition at line
        
         161
        
        of file
        
         em_rmu.h
        
        .
       
References _RMU_CTRL_RESETSTATE_MASK , _RMU_CTRL_RESETSTATE_SHIFT , and RMU .
| __STATIC_INLINE void RMU_UserResetStateSet | ( | uint32_t | 
            userState
            | ) | 
Set user reset state. Reset only by a Power-on-reset and a pin reset.
- Parameters
- 
         [in] userStateUser state to set 
        Definition at line
        
         146
        
        of file
        
         em_rmu.h
        
        .
       
References _RMU_CTRL_RESETSTATE_MASK , _RMU_CTRL_RESETSTATE_SHIFT , and RMU .