PRS_TypeDef Struct ReferenceDevices > EFR32MG13P932F512GM48 > Peripheral TypeDefsDevices > EFR32MG13P932F512GM48 > | Bit Fields > PRSDevices > | PRS
PRS Register Declaration
Definition at line
446
of file
efr32mg13p932f512gm48.h
.
#include <
efr32mg13p932f512gm48.h
>
Data Fields |
|
| PRS_CH_TypeDef | CH [12U] |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | DMAREQ0 |
| __IOM uint32_t | DMAREQ1 |
| __IM uint32_t | PEEK |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [5U] |
| uint32_t | RESERVED2 [1U] |
| uint32_t | RESERVED3 [3U] |
| __IOM uint32_t | ROUTELOC0 |
| __IOM uint32_t | ROUTELOC1 |
| __IOM uint32_t | ROUTELOC2 |
| __IOM uint32_t | ROUTEPEN |
| __IOM uint32_t | SWLEVEL |
| __IOM uint32_t | SWPULSE |
Field Documentation
| PRS_CH_TypeDef PRS_TypeDef::CH |
Channel registers
Definition at line
463
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::CTRL |
Control Register
Definition at line
456
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::DMAREQ0 |
DMA Request 0 Register
Definition at line
457
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::DMAREQ1 |
DMA Request 1 Register
Definition at line
458
of file
efr32mg13p932f512gm48.h
.
| __IM uint32_t PRS_TypeDef::PEEK |
PRS Channel Values
Definition at line
460
of file
efr32mg13p932f512gm48.h
.
| uint32_t PRS_TypeDef::RESERVED0 |
Reserved for future use
Definition at line
450
of file
efr32mg13p932f512gm48.h
.
| uint32_t PRS_TypeDef::RESERVED1 |
Reserved for future use
Definition at line
455
of file
efr32mg13p932f512gm48.h
.
| uint32_t PRS_TypeDef::RESERVED2 |
Reserved for future use
Definition at line
459
of file
efr32mg13p932f512gm48.h
.
| uint32_t PRS_TypeDef::RESERVED3 |
Reserved registers
Definition at line
462
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line
451
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::ROUTELOC1 |
I/O Routing Location Register
Definition at line
452
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::ROUTELOC2 |
I/O Routing Location Register
Definition at line
453
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::ROUTEPEN |
I/O Routing Pin Enable Register
Definition at line
449
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::SWLEVEL |
Software Level Register
Definition at line
448
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t PRS_TypeDef::SWPULSE |
Software Pulse Register
Definition at line
447
of file
efr32mg13p932f512gm48.h
.
The documentation for this struct was generated from the following files:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG13P/Include/
efr32mg13p932f512gm48.h -
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG13P/Include/
efr32mg13p_prs.h