USB_DOEP_TypeDef Struct ReferenceDevices
USB_DOEP EFM32HG USB DOEP.
Definition at line
45
of file
efm32hg_usb_doep.h
.
#include <
efm32hg_usb_doep.h
>
Data Fields |
|
| __IOM uint32_t | CTL |
| __IOM uint32_t | DMAADDR |
| __IOM uint32_t | INT |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [1U] |
| uint32_t | RESERVED2 [2U] |
| __IOM uint32_t | TSIZ |
Field Documentation
| __IOM uint32_t USB_DOEP_TypeDef::CTL |
Device OUT Endpoint x+1 Control Register
Definition at line
46
of file
efm32hg_usb_doep.h
.
| __IOM uint32_t USB_DOEP_TypeDef::DMAADDR |
Device OUT Endpoint x+1 DMA Address Register
Definition at line
51
of file
efm32hg_usb_doep.h
.
| __IOM uint32_t USB_DOEP_TypeDef::INT |
Device OUT Endpoint x+1 Interrupt Register
Definition at line
48
of file
efm32hg_usb_doep.h
.
| uint32_t USB_DOEP_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
47
of file
efm32hg_usb_doep.h
.
| uint32_t USB_DOEP_TypeDef::RESERVED1[1U] |
Reserved for future use
Definition at line
49
of file
efm32hg_usb_doep.h
.
| uint32_t USB_DOEP_TypeDef::RESERVED2[2U] |
Reserved future
Definition at line
52
of file
efm32hg_usb_doep.h
.
| __IOM uint32_t USB_DOEP_TypeDef::TSIZ |
Device OUT Endpoint x+1 Transfer Size Register
Definition at line
50
of file
efm32hg_usb_doep.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32HG/Include/
efm32hg_usb_doep.h