USBD_Callbacks_TypeDef Struct ReferencePlatform Middleware > USB > USB_DEVICE
USB Device stack callback structure.
Callback functions used by the device stack to signal events or query status to/from the application. See USBD_Init_TypeDef . Assign members to NULL if your application don't need a specific callback.
       Definition at line
       
        785
       
       of file
       
        em_usb.h
       
       .
      
      
       #include <
       
     
        em_usb.h
       
       >
      
         Data Fields | 
       |
| const USBD_IsSelfPoweredCb_TypeDef | isSelfPowered | 
| const USBD_SetupCmdCb_TypeDef | setupCmd | 
| const USBD_SofIntCb_TypeDef | sofInt | 
| const USBD_UsbResetCb_TypeDef | usbReset | 
| const USBD_DeviceStateChangeCb_TypeDef | usbStateChange | 
Field Documentation
| const USBD_IsSelfPoweredCb_TypeDef USBD_Callbacks_TypeDef::isSelfPowered | 
Called whenever the device stack needs to query if the device is currently self- or bus-powered. Applies to devices which can operate in both modes.
        Definition at line
        
         790
        
        of file
        
         em_usb.h
        
        .
       
| const USBD_SetupCmdCb_TypeDef USBD_Callbacks_TypeDef::setupCmd | 
Called on each setup request received from host.
        Definition at line
        
         789
        
        of file
        
         em_usb.h
        
        .
       
| const USBD_SofIntCb_TypeDef USBD_Callbacks_TypeDef::sofInt | 
Called at each SOF interrupt. If NULL, the device stack will not enable the SOF interrupt.
        Definition at line
        
         793
        
        of file
        
         em_usb.h
        
        .
       
| const USBD_UsbResetCb_TypeDef USBD_Callbacks_TypeDef::usbReset | 
Called whenever USB reset signalling is detected on the USB port.
        Definition at line
        
         786
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBX_init() .
| const USBD_DeviceStateChangeCb_TypeDef USBD_Callbacks_TypeDef::usbStateChange | 
Called whenever the device change state.
        Definition at line
        
         788
        
        of file
        
         em_usb.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/middleware/usb_gecko/inc/
       
em_usb.h