sleep.c File Reference

Energy Modes management driver.

License

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

Definition in file sleep.c .

#include " em_device.h "
#include " em_assert.h "
#include " em_core.h "
#include " em_rmu.h "
#include " em_emu.h "
#include " sleep.h "
#include <stdlib.h>

Functions

void SLEEP_ForceSleepInEM4 (void)
Force the device to go to EM4 without doing any checks.
void SLEEP_Init ( SLEEP_CbFuncPtr_t pSleepCb, SLEEP_CbFuncPtr_t pWakeUpCb)
Initialize the Sleep module.
void SLEEP_InitEx (const SLEEP_Init_t *init)
Initialize the Sleep module.
SLEEP_EnergyMode_t SLEEP_LowestEnergyModeGet (void)
Gets the lowest energy mode that the system is allowed to be set to.
SLEEP_EnergyMode_t SLEEP_Sleep (void)
Sets the system to sleep into the lowest possible energy mode.
void SLEEP_SleepBlockBegin ( SLEEP_EnergyMode_t eMode)
Begin sleep block in the requested energy mode.
void SLEEP_SleepBlockEnd ( SLEEP_EnergyMode_t eMode)
End sleep block in the requested energy mode.