MSDSCSI_RequestSenseData_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD
SCSI Request Sense response data typedef.
Definition at line
145
of file
msdscsi.h
.
#include <
msdscsi.h
>
Data Fields |
|
| struct { | |
| uint8_t ResponseCode : 7 | |
| uint8_t Valid : 1 | |
| }; | |
| struct { | |
| uint8_t Eom : 1 | |
| uint8_t FileMark : 1 | |
| uint8_t Ili : 1 | |
| uint8_t Reserved : 1 | |
| uint8_t SenseKey : 4 | |
| }; | |
| struct { | |
| uint8_t SenseKeySpecific1 : 7 | |
| uint8_t Sksv : 1 | |
| }; | |
| uint8_t | AdditionalLength |
| uint8_t | Asc |
| uint8_t | Ascq |
| uint32_t | CmdSpecificInfo |
| uint8_t | Fruc |
| uint32_t | Information |
| uint8_t | Obsolete |
| uint8_t | SenseKeySpecific2 |
| uint8_t | SenseKeySpecific3 |
Field Documentation
| uint8_t MSDSCSI_RequestSenseData_TypeDef::AdditionalLength |
Number of additional sense bytes that follow.
Definition at line
159
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Asc |
Additional sense code.
Definition at line
161
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Ascq |
Additional sense code qualifier.
Definition at line
162
of file
msdscsi.h
.
| uint32_t MSDSCSI_RequestSenseData_TypeDef::CmdSpecificInfo |
Command specific information field.
Definition at line
160
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Eom |
End of medium indicator.
Definition at line
155
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::FileMark |
Filemark indicator.
Definition at line
156
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Fruc |
Field replacable unit code.
Definition at line
163
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Ili |
Incorrect length indicator.
Definition at line
154
of file
msdscsi.h
.
| uint32_t MSDSCSI_RequestSenseData_TypeDef::Information |
Information field.
Definition at line
158
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Obsolete |
Obsolete, expect any value.
Definition at line
150
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Reserved |
Reserved, expect 0.
Definition at line
153
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::ResponseCode |
Response code, 0x70 = Current errors.
Definition at line
147
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKey |
Generic error information.
Definition at line
152
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific1 |
Sense key specific field.
Definition at line
165
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific2 |
Sense key specific field.
Definition at line
168
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific3 |
Sense key specific field.
Definition at line
169
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Sksv |
Sense key specific field qualifier.
Definition at line
166
of file
msdscsi.h
.
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Valid |
Valid, qualifier for Information field.
Definition at line
148
of file
msdscsi.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/hardware/kit/common/drivers/
msdscsi.h