UARTDRV_InitLeuart_t Struct ReferenceEMDRV > UARTDRV
LEUART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required to initialize a driver instance. This structure is passed to UARTDRV_InitLeuart() when initializing a UARTDRV instance.
Definition at line
219
of file
uartdrv.h
.
#include <
uartdrv.h
>
Data Fields |
|
uint32_t | baudRate |
UART baud rate.
|
|
uint8_t | ctsPin |
CTS pin number.
|
|
GPIO_Port_TypeDef | ctsPort |
CTS pin port number.
|
|
UARTDRV_FlowControlType_t | fcType |
Flow control mode.
|
|
LEUART_Parity_TypeDef | parity |
Parity configuration.
|
|
LEUART_TypeDef * | port |
The peripheral used for LEUART.
|
|
uint8_t | portLocation |
Location number for LEUART pins.
|
|
uint8_t | rtsPin |
RTS pin number.
|
|
GPIO_Port_TypeDef | rtsPort |
RTS pin port number.
|
|
UARTDRV_Buffer_FifoQueue_t * | rxQueue |
Receive operation queue.
|
|
LEUART_Stopbits_TypeDef | stopBits |
Number of stop bits.
|
|
UARTDRV_Buffer_FifoQueue_t * | txQueue |
Transmit operation queue.
|
|
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emdrv/uartdrv/inc/
uartdrv.h