TEXTDISPLAY_Config_t Struct ReferenceKit Drivers > Textdisplay
Initialization data structure for text display devices.
Definition at line
69
of file
textdisplay.h
.
#include <
textdisplay.h
>
Data Fields |
|
| int | displayDeviceNo |
| bool | lfToCrLf |
| bool | scrollEnable |
Field Documentation
| int TEXTDISPLAY_Config_t::displayDeviceNo |
Display device number to initialize test display on.
Definition at line
70
of file
textdisplay.h
.
Referenced by RETARGET_TextDisplayInit() , and TEXTDISPLAY_New() .
| bool TEXTDISPLAY_Config_t::lfToCrLf |
Enable or disable LF to CR+LF conversion.
Definition at line
77
of file
textdisplay.h
.
Referenced by RETARGET_TextDisplayInit() , and TEXTDISPLAY_New() .
| bool TEXTDISPLAY_Config_t::scrollEnable |
Enable/disable scrolling mode on the text display. Scrolling mode will consume more memory because the lines will have to be stored in memory.
Definition at line
72
of file
textdisplay.h
.
Referenced by RETARGET_TextDisplayInit() , and TEXTDISPLAY_New() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/hardware/kit/common/drivers/
textdisplay.h