ADC_InitSingle_TypeDef Struct ReferenceEMLIB > ADC
Single conversion initialization structure.
Definition at line
964
of file
em_adc.h
.
#include <
em_adc.h
>
Data Fields |
|
| ADC_AcqTime_TypeDef | acqTime |
| bool | diff |
| bool | fifoOverwrite |
| bool | leftAdjust |
| ADC_NegSel_TypeDef | negSel |
| ADC_PosSel_TypeDef | posSel |
| bool | prsEnable |
| ADC_PRSSEL_TypeDef | prsSel |
| ADC_Ref_TypeDef | reference |
| bool | rep |
| ADC_Res_TypeDef | resolution |
| bool | singleDmaEm2Wu |
Field Documentation
| ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
Definition at line
972
of file
em_adc.h
.
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and adcInit() .
| bool ADC_InitSingle_TypeDef::diff |
Select if single-ended or differential input.
Definition at line
1003
of file
em_adc.h
.
Referenced by ADC_InitSingle() .
| bool ADC_InitSingle_TypeDef::fifoOverwrite |
When true, FIFO overwrites old data when full. If false, FIFO discards new data. The SCANOF IRQ is triggered in both cases.
Definition at line
1022
of file
em_adc.h
.
Referenced by ADC_InitSingle() .
| bool ADC_InitSingle_TypeDef::leftAdjust |
Select if left adjustment should be done.
Definition at line
1009
of file
em_adc.h
.
Referenced by ADC_InitSingle() .
| ADC_NegSel_TypeDef ADC_InitSingle_TypeDef::negSel |
Select negative input for single channel conversion mode. Negative input is grounded for single-ended (non-differential) converison.
Definition at line
999
of file
em_adc.h
.
Referenced by ADC_InitSingle() , and adcInit() .
| ADC_PosSel_TypeDef ADC_InitSingle_TypeDef::posSel |
Select positive input for single channel conversion mode.
Definition at line
993
of file
em_adc.h
.
Referenced by ADC_InitSingle() , and adcInit() .
| bool ADC_InitSingle_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
Definition at line
1006
of file
em_adc.h
.
Referenced by ADC_InitSingle() , and adcInit() .
| ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if
prsEnable
is enabled.
Definition at line
969
of file
em_adc.h
.
Referenced by ADC_InitSingle() , and adcInit() .
| ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference |
Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.
Definition at line
978
of file
em_adc.h
.
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , adcInit() , and TOUCH_Init() .
| bool ADC_InitSingle_TypeDef::rep |
Select if continuous conversion until explicit stop.
Definition at line
1012
of file
em_adc.h
.
Referenced by ADC_InitSingle() .
| ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution |
Sample resolution.
Definition at line
981
of file
em_adc.h
.
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and TOUCH_Init() .
| bool ADC_InitSingle_TypeDef::singleDmaEm2Wu |
When true, DMA is available in EM2 for single conversion
Definition at line
1016
of file
em_adc.h
.
Referenced by ADC_InitSingle() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_adc.h