SMU_Init_TypeDef Struct ReferenceEMLIB > SMU

SMU initialization structure.

Definition at line 814 of file em_smu.h .

#include < em_smu.h >

Data Fields

bool enable
union {
SMU_PrivilegedAccess_TypeDef access
uint32_t reg [2]
} ppu

Field Documentation

SMU_PrivilegedAccess_TypeDef SMU_Init_TypeDef::access

Peripheral access control array.

Definition at line 817 of file em_smu.h .

bool SMU_Init_TypeDef::enable

SMU enable flag. When set, SMU_Init() will enable SMU.

Definition at line 819 of file em_smu.h .

Referenced by SMU_Init() .

uint32_t SMU_Init_TypeDef::reg[2]

Peripheral access control array.

Definition at line 816 of file em_smu.h .

Referenced by SMU_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/ em_smu.h