SensorStruct_t Struct ReferencePlatform Middleware > Capacitive Sensing Firmware Library

Stores all runtime values for an enabled capacitive sensor.

Definition at line 71 of file cslib.h .

#include < cslib.h >

Data Fields

uint8_t activeIndicator
Bit array showing whether touch is qualified on sensor, uses DEBOUNCE_ACTIVE_MASK.
signed char baselineAccumulator
Tracks trend of CS values to determine whether baseline rises or falls.
uint32_t currentBaseline
Runtime estimate of untouched or inactive state of CS sensor input.
uint8_t debounceCounts
Stores consecutive CS values above or below active or inactive threshold.
SI_UU32_t expValue
Filtered CS value with 16 bits of LSBs.
uint32_t rawBuffer [ DEF_SENSOR_BUFFER_SIZE ]
Newest sample taken from CS hardware, without any processing.
uint8_t touchDeltaDiv16
Describes the expected difference between untouched and touched CS value.

The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/middleware/cslib/inc/ cslib.h