ADCEMLIB
Detailed Description
Analog to Digital Converter (ADC) Peripheral API.
This module contains functions to control the ADC peripheral of Silicon Labs 32-bit MCUs and SoCs. The ADC is used to convert analog signals into a digital representation.
Data Structures | |
struct | ADC_Init_TypeDef |
struct | ADC_InitScan_TypeDef |
struct | ADC_InitScanInput_TypeDef |
struct | ADC_InitSingle_TypeDef |
Macros | |
#define | ADC_INIT_DEFAULT |
#define | ADC_INITSCAN_DEFAULT |
#define | ADC_INITSINGLE_DEFAULT |
Enumerations | |
enum | ADC_AcqTime_TypeDef { adcAcqTime1 = _ADC_SINGLECTRL_AT_1CYCLE, adcAcqTime2 = _ADC_SINGLECTRL_AT_2CYCLES, adcAcqTime4 = _ADC_SINGLECTRL_AT_4CYCLES, adcAcqTime8 = _ADC_SINGLECTRL_AT_8CYCLES, adcAcqTime16 = _ADC_SINGLECTRL_AT_16CYCLES, adcAcqTime32 = _ADC_SINGLECTRL_AT_32CYCLES, adcAcqTime64 = _ADC_SINGLECTRL_AT_64CYCLES, adcAcqTime128 = _ADC_SINGLECTRL_AT_128CYCLES, adcAcqTime256 = _ADC_SINGLECTRL_AT_256CYCLES } |
enum | ADC_LPFilter_TypeDef { adcLPFilterBypass = _ADC_CTRL_LPFMODE_BYPASS, adcLPFilterRC = _ADC_CTRL_LPFMODE_RCFILT, adcLPFilterDeCap = _ADC_CTRL_LPFMODE_DECAP } |
enum | ADC_OvsRateSel_TypeDef { adcOvsRateSel2 = _ADC_CTRL_OVSRSEL_X2, adcOvsRateSel4 = _ADC_CTRL_OVSRSEL_X4, adcOvsRateSel8 = _ADC_CTRL_OVSRSEL_X8, adcOvsRateSel16 = _ADC_CTRL_OVSRSEL_X16, adcOvsRateSel32 = _ADC_CTRL_OVSRSEL_X32, adcOvsRateSel64 = _ADC_CTRL_OVSRSEL_X64, adcOvsRateSel128 = _ADC_CTRL_OVSRSEL_X128, adcOvsRateSel256 = _ADC_CTRL_OVSRSEL_X256, adcOvsRateSel512 = _ADC_CTRL_OVSRSEL_X512, adcOvsRateSel1024 = _ADC_CTRL_OVSRSEL_X1024, adcOvsRateSel2048 = _ADC_CTRL_OVSRSEL_X2048, adcOvsRateSel4096 = _ADC_CTRL_OVSRSEL_X4096 } |
enum | ADC_PRSSEL_TypeDef { adcPRSSELCh0 = _ADC_SINGLECTRL_PRSSEL_PRSCH0, adcPRSSELCh1 = _ADC_SINGLECTRL_PRSSEL_PRSCH1, adcPRSSELCh2 = _ADC_SINGLECTRL_PRSSEL_PRSCH2, adcPRSSELCh3 = _ADC_SINGLECTRL_PRSSEL_PRSCH3, adcPRSSELCh4 = _ADC_SINGLECTRL_PRSSEL_PRSCH4, adcPRSSELCh5 = _ADC_SINGLECTRL_PRSSEL_PRSCH5, adcPRSSELCh6 = _ADC_SINGLECTRL_PRSSEL_PRSCH6, adcPRSSELCh7 = _ADC_SINGLECTRL_PRSSEL_PRSCH7 } |
enum | ADC_Ref_TypeDef { adcRef1V25 = _ADC_SINGLECTRL_REF_1V25, adcRef2V5 = _ADC_SINGLECTRL_REF_2V5, adcRefVDD = _ADC_SINGLECTRL_REF_VDD, adcRef5VDIFF = _ADC_SINGLECTRL_REF_5VDIFF, adcRefExtSingle = _ADC_SINGLECTRL_REF_EXTSINGLE, adcRef2xExtDiff = _ADC_SINGLECTRL_REF_2XEXTDIFF, adcRef2xVDD = _ADC_SINGLECTRL_REF_2XVDD } |
enum | ADC_Res_TypeDef { adcRes12Bit = _ADC_SINGLECTRL_RES_12BIT, adcRes8Bit = _ADC_SINGLECTRL_RES_8BIT, adcRes6Bit = _ADC_SINGLECTRL_RES_6BIT, adcResOVS = _ADC_SINGLECTRL_RES_OVS } |
enum | ADC_SingleInput_TypeDef { adcSingleInputCh0 = _ADC_SINGLECTRL_INPUTSEL_CH0, adcSingleInputCh1 = _ADC_SINGLECTRL_INPUTSEL_CH1, adcSingleInputCh2 = _ADC_SINGLECTRL_INPUTSEL_CH2, adcSingleInputCh3 = _ADC_SINGLECTRL_INPUTSEL_CH3, adcSingleInputCh4 = _ADC_SINGLECTRL_INPUTSEL_CH4, adcSingleInputCh5 = _ADC_SINGLECTRL_INPUTSEL_CH5, adcSingleInputCh6 = _ADC_SINGLECTRL_INPUTSEL_CH6, adcSingleInputCh7 = _ADC_SINGLECTRL_INPUTSEL_CH7, adcSingleInputTemp = _ADC_SINGLECTRL_INPUTSEL_TEMP, adcSingleInputVDDDiv3 = _ADC_SINGLECTRL_INPUTSEL_VDDDIV3, adcSingleInputVDD = _ADC_SINGLECTRL_INPUTSEL_VDD, adcSingleInputVSS = _ADC_SINGLECTRL_INPUTSEL_VSS, adcSingleInputVrefDiv2 = _ADC_SINGLECTRL_INPUTSEL_VREFDIV2, adcSingleInputDACOut0 = _ADC_SINGLECTRL_INPUTSEL_DAC0OUT0, adcSingleInputDACOut1 = _ADC_SINGLECTRL_INPUTSEL_DAC0OUT1, adcSingleInputATEST = 15, adcSingleInputCh0Ch1 = _ADC_SINGLECTRL_INPUTSEL_CH0CH1, adcSingleInputCh2Ch3 = _ADC_SINGLECTRL_INPUTSEL_CH2CH3, adcSingleInputCh4Ch5 = _ADC_SINGLECTRL_INPUTSEL_CH4CH5, adcSingleInputCh6Ch7 = _ADC_SINGLECTRL_INPUTSEL_CH6CH7, adcSingleInputDiff0 = 4 } |
enum | ADC_Start_TypeDef { adcStartSingle = ADC_CMD_SINGLESTART, adcStartScan = ADC_CMD_SCANSTART, adcStartScanAndSingle = ADC_CMD_SCANSTART | ADC_CMD_SINGLESTART } |
enum | ADC_Warmup_TypeDef { adcWarmupNormal = _ADC_CTRL_WARMUPMODE_NORMAL, adcWarmupFastBG = _ADC_CTRL_WARMUPMODE_FASTBG, adcWarmupKeepScanRefWarm = _ADC_CTRL_WARMUPMODE_KEEPSCANREFWARM, adcWarmupKeepADCWarm = _ADC_CTRL_WARMUPMODE_KEEPADCWARM } |
Functions | |
__STATIC_INLINE uint32_t | ADC_DataScanGet (ADC_TypeDef *adc) |
Get a scan result. | |
__STATIC_INLINE uint32_t | ADC_DataScanPeek (ADC_TypeDef *adc) |
Peek scan result. | |
__STATIC_INLINE uint32_t | ADC_DataSingleGet (ADC_TypeDef *adc) |
Get a single conversion result. | |
__STATIC_INLINE uint32_t | ADC_DataSinglePeek (ADC_TypeDef *adc) |
Peek single conversion result. | |
void | ADC_Init (ADC_TypeDef *adc, const ADC_Init_TypeDef *init) |
Initialize ADC. | |
void | ADC_InitScan (ADC_TypeDef *adc, const ADC_InitScan_TypeDef *init) |
Initialize the ADC scan sequence. | |
void | ADC_InitSingle (ADC_TypeDef *adc, const ADC_InitSingle_TypeDef *init) |
Initialize the single ADC sample conversion. | |
__STATIC_INLINE void | ADC_IntClear (ADC_TypeDef *adc, uint32_t flags) |
Clear one or more pending ADC interrupts. | |
__STATIC_INLINE void | ADC_IntDisable (ADC_TypeDef *adc, uint32_t flags) |
Disable one or more ADC interrupts. | |
__STATIC_INLINE void | ADC_IntEnable (ADC_TypeDef *adc, uint32_t flags) |
Enable one or more ADC interrupts. | |
__STATIC_INLINE uint32_t | ADC_IntGet (ADC_TypeDef *adc) |
Get pending ADC interrupt flags. | |
__STATIC_INLINE uint32_t | ADC_IntGetEnabled (ADC_TypeDef *adc) |
Get enabled and pending ADC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler. | |
__STATIC_INLINE void | ADC_IntSet (ADC_TypeDef *adc, uint32_t flags) |
Set one or more pending ADC interrupts from software. | |
uint8_t | ADC_PrescaleCalc (uint32_t adcFreq, uint32_t hfperFreq) |
Calculate the prescaler value used to determine the ADC clock. | |
void | ADC_Reset (ADC_TypeDef *adc) |
Reset ADC to a state that it was in after a hardware reset. | |
__STATIC_INLINE void | ADC_Start (ADC_TypeDef *adc, ADC_Start_TypeDef cmd) |
Start scan sequence and/or single conversion. | |
uint8_t | ADC_TimebaseCalc (uint32_t hfperFreq) |
Calculate a timebase value to get a timebase providing at least 1 us. | |
Macro Definition Documentation
#define ADC_INIT_DEFAULT |
Default configuration for ADC initialization structure.
Definition at line 821
of file em_adc.h
.
Referenced by adcInit(), MIC_init(), and TOUCH_Init().
#define ADC_INITSCAN_DEFAULT |
Default configuration for ADC scan initialization structure.
Definition at line 927
of file em_adc.h
.
Referenced by MIC_init().
#define ADC_INITSINGLE_DEFAULT |
Default configuration for ADC single conversion initialization structure.
Definition at line 1028
of file em_adc.h
.
Referenced by adcInit().
Enumeration Type Documentation
enum ADC_AcqTime_TypeDef |
Acquisition time (in ADC clock cycles).
Definition at line 59
of file em_adc.h
.
enum ADC_LPFilter_TypeDef |
Oversample rate select.
Definition at line 86
of file em_adc.h
.
enum ADC_PRSSEL_TypeDef |
Peripheral Reflex System signal used to trigger a single sample.
Definition at line 125
of file em_adc.h
.
enum ADC_Ref_TypeDef |
Single and scan mode voltage references. Using unshifted enumerations and or in ADC_CTRLX_VREFSEL_REG to select the extension register CTRLX_VREFSEL.
Definition at line 190
of file em_adc.h
.
enum ADC_Res_TypeDef |
Single sample input selection.
Definition at line 275
of file em_adc.h
.
enum ADC_Start_TypeDef |
enum ADC_Warmup_TypeDef |
Warm-up mode.
Definition at line 738
of file em_adc.h
.
Function Documentation
__STATIC_INLINE uint32_t ADC_DataScanGet | ( | ADC_TypeDef * | adc | ) |
Get a scan result.
- Note
- Check data valid flag before calling this function.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block.
- Returns
- Scan conversion data.
Definition at line 1111
of file em_adc.h
.
__STATIC_INLINE uint32_t ADC_DataScanPeek | ( | ADC_TypeDef * | adc | ) |
Peek scan result.
- Note
- Check data valid flag before calling this function.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block.
- Returns
- Scan conversion data.
Definition at line 1129
of file em_adc.h
.
__STATIC_INLINE uint32_t ADC_DataSingleGet | ( | ADC_TypeDef * | adc | ) |
Get a single conversion result.
- Note
- Check data valid flag before calling this function.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block.
- Returns
- Single conversion data.
Definition at line 1075
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), and getAdcSample().
__STATIC_INLINE uint32_t ADC_DataSinglePeek | ( | ADC_TypeDef * | adc | ) |
Peek single conversion result.
- Note
- Check data valid flag before calling this function.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block.
- Returns
- Single conversion data.
Definition at line 1093
of file em_adc.h
.
void ADC_Init | ( | ADC_TypeDef * | adc, |
const ADC_Init_TypeDef * | init |
||
) |
Initialize ADC.
Initializes common parts for both single conversion and scan sequence. In addition, single and/or scan control configuration must be done. See ADC_InitSingle() and ADC_InitScan() respectively. For ADC architectures with the ADCn->SCANINPUTSEL register, use ADC_ScanSingleEndedInputAdd() to configure single-ended scan inputs or ADC_ScanDifferentialInputAdd() to configure differential scan inputs. ADC_ScanInputClear() is also provided for applications that need to update the input configuration.
- Note
- This function will stop any ongoing conversion.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block. [in] init
A pointer to the ADC initialization structure.
Definition at line 379
of file em_adc.c
.
References ADC_IntClear(), ADC_PrescaleCalc(), BUS_RegMaskedWrite(), CMU_ClockFreqGet(), cmuClock_ADC0, ADC_Init_TypeDef::lpfMode, ADC_Init_TypeDef::ovsRateSel, ADC_Init_TypeDef::prescale, ADC_Init_TypeDef::tailgate, ADC_Init_TypeDef::timebase, and ADC_Init_TypeDef::warmUpMode.
Referenced by adcInit(), MIC_init(), and TOUCH_Init().
void ADC_InitScan | ( | ADC_TypeDef * | adc, |
const ADC_InitScan_TypeDef * | init |
||
) |
Initialize the ADC scan sequence.
See ADC_Start() for starting a scan sequence.
When selecting an external reference, the gain and offset calibration must be set explicitly (CAL register). For other references, the calibration is updated with values defined during manufacturing. For ADC architectures with the ADCn->SCANINPUTSEL register, use ADC_ScanSingleEndedInputAdd() to configure single-ended scan inputs or ADC_ScanDifferentialInputAdd() to configure differential scan inputs. ADC_ScanInputClear() is also provided for applications that need to update the input configuration.
- Note
- This function will stop any ongoing scan sequence.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block. [in] init
A pointer to the ADC initialization structure.
Definition at line 710
of file em_adc.c
.
References ADC_InitScan_TypeDef::acqTime, BUS_RegBitWrite(), ADC_InitScan_TypeDef::diff, ADC_InitScan_TypeDef::input, ADC_InitScan_TypeDef::leftAdjust, ADC_InitScan_TypeDef::prsEnable, ADC_InitScan_TypeDef::prsSel, ADC_InitScan_TypeDef::reference, ADC_InitScan_TypeDef::rep, and ADC_InitScan_TypeDef::resolution.
Referenced by MIC_init().
void ADC_InitSingle | ( | ADC_TypeDef * | adc, |
const ADC_InitSingle_TypeDef * | init |
||
) |
Initialize the single ADC sample conversion.
See ADC_Start() for starting a single conversion.
When selecting an external reference, the gain and offset calibration must be set explicitly (CAL register). For other references, the calibration is updated with values defined during manufacturing.
- Note
- This function will stop any ongoing single conversion.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block. [in] init
A pointer to the ADC initialization structure.
Definition at line 847
of file em_adc.c
.
References ADC_InitSingle_TypeDef::acqTime, adcAcqTime8, adcRef1V25, BUS_RegBitWrite(), ADC_InitSingle_TypeDef::diff, ADC_InitSingle_TypeDef::input, ADC_InitSingle_TypeDef::leftAdjust, ADC_InitSingle_TypeDef::prsEnable, ADC_InitSingle_TypeDef::prsSel, ADC_InitSingle_TypeDef::reference, ADC_InitSingle_TypeDef::rep, and ADC_InitSingle_TypeDef::resolution.
Referenced by ADC0_IRQHandler(), adcInit(), and TOUCH_Init().
__STATIC_INLINE void ADC_IntClear | ( | ADC_TypeDef * | adc, |
uint32_t | flags |
||
) |
Clear one or more pending ADC interrupts.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block. [in] flags
Pending ADC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).
Definition at line 1168
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), ADC_Init(), and TOUCH_Init().
__STATIC_INLINE void ADC_IntDisable | ( | ADC_TypeDef * | adc, |
uint32_t | flags |
||
) |
Disable one or more ADC interrupts.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block. [in] flags
ADC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).
Definition at line 1184
of file em_adc.h
.
Referenced by TOUCH_GetPos(), and TOUCH_Init().
__STATIC_INLINE void ADC_IntEnable | ( | ADC_TypeDef * | adc, |
uint32_t | flags |
||
) |
Enable one or more ADC interrupts.
- Note
- Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using ADC_IntClear() prior to enabling if the pending interrupt should be ignored.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block. [in] flags
ADC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).
Definition at line 1205
of file em_adc.h
.
Referenced by TOUCH_GetPos(), and TOUCH_Init().
__STATIC_INLINE uint32_t ADC_IntGet | ( | ADC_TypeDef * | adc | ) |
Get pending ADC interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block.
- Returns
- ADC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).
Definition at line 1224
of file em_adc.h
.
Referenced by getAdcSample().
__STATIC_INLINE uint32_t ADC_IntGetEnabled | ( | ADC_TypeDef * | adc | ) |
Get enabled and pending ADC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block.
- Note
- This function does not clear interrupt flags.
- Returns
- Pending and enabled ADC interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in ADCx_IEN_nnn register (ADCx_IEN_nnn) and
- the OR combination of valid interrupt flags of the ADC module (ADCx_IF_nnn).
Definition at line 1248
of file em_adc.h
.
__STATIC_INLINE void ADC_IntSet | ( | ADC_TypeDef * | adc, |
uint32_t | flags |
||
) |
Set one or more pending ADC interrupts from software.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block. [in] flags
ADC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).
Definition at line 1271
of file em_adc.h
.
uint8_t ADC_PrescaleCalc | ( | uint32_t | adcFreq, |
uint32_t | hfperFreq |
||
) |
Calculate the prescaler value used to determine the ADC clock.
The ADC clock is given by: (HFPERCLK or HFPERCCLK) / (prescale + 1).
- Note
- The return value is clamped to the maximum prescaler value that the hardware supports.
- Parameters
-
[in] adcFreq
ADC frequency wanted. The frequency will automatically be adjusted to a valid range according to the reference manual. [in] hfperFreq
Frequency in Hz of reference HFPER/HFPERC clock. Set to 0 to use currently defined HFPER/HFPERC clock setting.
- Returns
- A prescaler value to use for ADC in order to achieve a clock value <=
adcFreq
.
Definition at line 1009
of file em_adc.c
.
References CMU_ClockFreqGet(), and cmuClock_HFPER.
Referenced by ADC_Init(), adcInit(), MIC_init(), and TOUCH_Init().
void ADC_Reset | ( | ADC_TypeDef * | adc | ) |
Reset ADC to a state that it was in after a hardware reset.
- Note
- The ROUTE register is NOT reset by this function to allow a centralized setup of this feature.
- Parameters
-
[in] adc
A pointer to ADC peripheral register block.
Definition at line 1054
of file em_adc.c
.
References adcRef1V25.
__STATIC_INLINE void ADC_Start | ( | ADC_TypeDef * | adc, |
ADC_Start_TypeDef | cmd |
||
) |
Start scan sequence and/or single conversion.
- Parameters
-
[in] adc
A pointer to the ADC peripheral register block. [in] cmd
A command indicating which type of sampling to start.
Definition at line 1286
of file em_adc.h
.
Referenced by ADC0_IRQHandler(), getAdcSample(), and TOUCH_Init().
uint8_t ADC_TimebaseCalc | ( | uint32_t | hfperFreq | ) |
Calculate a timebase value to get a timebase providing at least 1 us.
- Parameters
-
[in] hfperFreq
Frequency in Hz of the reference HFPER/HFPERC clock. Set to 0 to use currently defined HFPER/HFPERC clock setting.
- Returns
- A timebase value to use for ADC to achieve at least 1 us.
Definition at line 1105
of file em_adc.c
.
References CMU_ClockFreqGet(), and cmuClock_HFPER.
Referenced by adcInit(), and MIC_init().