SegmentLcdKit Drivers

Detailed Description

Segment LCD driver.

This driver implements symbol and string write support for EFM32 kits with segment LCD.

Data Structures

struct  ARING_TypeDef
 Defines segment COM and BIT fields for A-wheel (suited for Anim)
 
struct  ARRAY_TypeDef
 Defines segment COM and BIT fields for array.
 
struct  BATTERY_TypeDef
 Defines segment COM and BIT fields for Battery (suited for Anim)
 
struct  Block_TypeDef
 Defines segment COM and BIT fields for top and bottom row blocks. The bit pattern shown above for characters can be split into upper and lower portions for animation purposes. There are separate COM and BIT numbers which together represent a set of stacked blocks which can be shown on two rows in the segmented LCD screen.
 
struct  CHAR_TypeDef
 Defines each text symbol's segment in terms of COM and BIT numbers, in a way that we can enumerate each bit for each text segment in the following bit pattern:
 
struct  EM_TypeDef
 Defines segment COM and BIT fields for Energy Modes on display.
 
struct  MCU_DISPLAY
 Defines prototype for all segments in display.
 
struct  NUMBER_TypeDef
 Defines segment COM and BIT fields numeric display.
 

Macros

#define ALPHA_DIGITS   7
 
#define ALPHA_VAL_MAX   9999999
 
#define ALPHA_VAL_MIN   -9999999
 
#define NUM_DIGITS   4
 
#define NUM_VAL_MAX   9999
 
#define NUM_VAL_MAX_HEX   0xFFFF
 
#define NUM_VAL_MIN   -999
 
#define SEGMENT_LCD_BLOCK_MODE_BLANK   0
 
#define SEGMENT_LCD_BLOCK_MODE_FILL   1
 
#define SEGMENT_LCD_BLOCK_MODE_OUTLINE   2
 
#define SEGMENT_LCD_BLOCK_MODE_OUTLINE_FILL   3
 
#define SEGMENT_LCD_NUM_BLOCK_COLUMNS   7
 

Enumerations

enum  SegmentLCD_BlockMode_TypeDef {
  segmentLCDBlockModeBlank = SEGMENT_LCD_BLOCK_MODE_BLANK,
  segmentLCDBlockModeFill = SEGMENT_LCD_BLOCK_MODE_FILL,
  segmentLCDBlockModeOutline = SEGMENT_LCD_BLOCK_MODE_OUTLINE,
  segmentLCDBlockModeOutlineFill = SEGMENT_LCD_BLOCK_MODE_OUTLINE_FILL
}
 

Functions

static void displayBlock (SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS])
 Working instance of LCD display.
 
void SegmentLCD_AllOff (void)
 Disable all segments.
 
void SegmentLCD_AllOn (void)
 Enable all segments.
 
void SegmentLCD_AlphaNumberOff (void)
 Turn all segments on alpha characters in display off.
 
void SegmentLCD_ARing (int anum, int on)
 Light up or shut off Ring of Indicators.
 
void SegmentLCD_Battery (int batteryLevel)
 Light up or shut off Battery Indicator.
 
void SegmentLCD_Block (SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS])
 
void SegmentLCD_Disable (void)
 Disables LCD controller.
 
void SegmentLCD_EnergyMode (int em, int on)
 Light up or shut off Energy Mode indicator.
 
void SegmentLCD_Init (bool useBoost)
 Segment LCD Initialization routine for EFM32 STK display.
 
void SegmentLCD_LowerHex (uint32_t num)
 Write a hexadecimal number on lower alphanumeric part of Segment LCD display.
 
void SegmentLCD_LowerNumber (int num)
 Write number on lower alphanumeric part of Segment LCD display.
 
void SegmentLCD_Number (int value)
 Write number on numeric part on Segment LCD display.
 
void SegmentLCD_NumberOff (void)
 Turn all segments on numeric digits in display off.
 
unsigned int SegmentLCD_segCnt (unsigned int segdl, unsigned int segdh)
 Counting the number of active segments in a single common line.
 
void SegmentLCD_Symbol (lcdSymbol s, int on)
 Light up or shut off various symbols on Segment LCD.
 
void SegmentLCD_UnsignedHex (uint32_t value)
 Write hexadecimal number on numeric part on Segment LCD display.
 
void SegmentLCD_Write (const char *string)
 Write text on LCD display.
 

Variables

static const uint16_t Blocks []
 Defines highlighted segments for the block display.
 
static const MCU_DISPLAY EFM_Display = EFM_DISPLAY_DEF
 Working instance of LCD display.
 
static const uint16_t Segment_Alphabet []
 Defines higlighted segments for the alphabet, starting from "blank" (SPACE) Uses bit pattern as defined for text segments above. E.g. a capital O, would have bits 0 1 2 3 4 5 => 0x003f defined.
 
static const uint16_t Segment_Numbers []
 Defines higlighted segments for the numeric display.
 

Enumeration Type Documentation

Enumerator
segmentLCDBlockModeBlank 

Blank

segmentLCDBlockModeFill 

Fill

segmentLCDBlockModeOutline 

Outline

segmentLCDBlockModeOutlineFill 

Outline and fill

Definition at line 52 of file segmentlcd.h.

Function Documentation

static void displayBlock ( SegmentLCD_BlockMode_TypeDef  topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS],
SegmentLCD_BlockMode_TypeDef  botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS] 
)
static

Working instance of LCD display.

Enabling/disabling dynamic charge redistribution.

Parameters
true==> enable, false ==> disable

Dynamically switching charge redistribution ON/OFF based on display contents

Parameters
None

Definition at line 1310 of file segmentlcd.c.

References Block_TypeDef::bit, Blocks, MCU_DISPLAY::BotBlocks, Block_TypeDef::com, LCD_SegmentSet(), and MCU_DISPLAY::TopBlocks.

void SegmentLCD_ARing ( int  anum,
int  on 
)

Light up or shut off Ring of Indicators.

Parameters
anum"Segment number" on "Ring", range 0 - 7
onZero is off, non-zero is on

Definition at line 1378 of file segmentlcd.c.

References MCU_DISPLAY::ARing, ARING_TypeDef::bit, ARING_TypeDef::com, and LCD_SegmentSet().

void SegmentLCD_Battery ( int  batteryLevel)

Light up or shut off Battery Indicator.

Parameters
batteryLevelBattery Level, 0 to 4 (0 turns all off)

Definition at line 1396 of file segmentlcd.c.

References MCU_DISPLAY::Battery, BATTERY_TypeDef::bit, BATTERY_TypeDef::com, and LCD_SegmentSet().

void SegmentLCD_EnergyMode ( int  em,
int  on 
)

Light up or shut off Energy Mode indicator.

Parameters
emEnergy Mode numer 0 to 4
onZero is off, non-zero is on

Definition at line 1423 of file segmentlcd.c.

References EM_TypeDef::bit, EM_TypeDef::com, MCU_DISPLAY::EMode, and LCD_SegmentSet().

void SegmentLCD_Init ( bool  useBoost)

Segment LCD Initialization routine for EFM32 STK display.

Parameters
useBoostSet to use voltage boost

Definition at line 465 of file segmentlcd.c.

References CMU_ClockDivSet(), CMU_ClockEnable(), CMU_ClockSelectSet(), CMU_LCDClkFDIVSet(), cmuClock_LCD, cmuClock_LCDpre, cmuClock_LFA, cmuSelect_LFRCO, LCD_Init(), LCD_IntDisable(), LCD_SyncBusyDelay(), LCD_VBoostSet(), LCD_VLCDSelect(), lcdVLCDSelVExtBoost, and SegmentLCD_AllOff().

void SegmentLCD_LowerHex ( uint32_t  num)

Write a hexadecimal number on lower alphanumeric part of Segment LCD display.

Parameters
numHexadecimal number value to put on display, in range 0 to 0x0FFFFFFF

Definition at line 519 of file segmentlcd.c.

References SegmentLCD_Symbol(), and SegmentLCD_Write().

void SegmentLCD_LowerNumber ( int  num)

Write number on lower alphanumeric part of Segment LCD display.

Parameters
numNumeric value to put on display, in range -9999999 to +9999999

Definition at line 552 of file segmentlcd.c.

References SegmentLCD_Symbol(), and SegmentLCD_Write().

void SegmentLCD_Number ( int  value)

Write number on numeric part on Segment LCD display.

Parameters
valueNumeric value to put on display, in range -999 to +9999

Definition at line 597 of file segmentlcd.c.

References NUMBER_TypeDef::bit, NUMBER_TypeDef::com, LCD_FreezeEnable(), LCD_SegmentSet(), LCD_SyncBusyDelay(), MCU_DISPLAY::Number, Segment_Numbers, and SegmentLCD_NumberOff().

unsigned int SegmentLCD_segCnt ( unsigned int  segdl,
unsigned int  segdh 
)

Counting the number of active segments in a single common line.

Parameters
valuein registers LCD_SEGDnL and LCD_SEGDnH (n = common line number)

Definition at line 1137 of file segmentlcd.c.

void SegmentLCD_Symbol ( lcdSymbol  s,
int  on 
)

Light up or shut off various symbols on Segment LCD.

Parameters
sWhich symbol to turn on or off
onZero is off, non-zero is on

Definition at line 678 of file segmentlcd.c.

References LCD_SegmentSet().

Referenced by SegmentLCD_LowerHex(), and SegmentLCD_LowerNumber().

void SegmentLCD_UnsignedHex ( uint32_t  value)

Write hexadecimal number on numeric part on Segment LCD display.

Parameters
valueNumeric value to put on display

Definition at line 1032 of file segmentlcd.c.

References NUMBER_TypeDef::bit, NUMBER_TypeDef::com, LCD_FreezeEnable(), LCD_SegmentSet(), LCD_SyncBusyDelay(), MCU_DISPLAY::Number, Segment_Numbers, and SegmentLCD_NumberOff().

void SegmentLCD_Write ( const char *  string)

Write text on LCD display.

Parameters
stringText string to show on display

Definition at line 1079 of file segmentlcd.c.

References CHAR_TypeDef::bit, CHAR_TypeDef::com, LCD_FreezeEnable(), LCD_SegmentSet(), LCD_SyncBusyDelay(), Segment_Alphabet, SegmentLCD_AlphaNumberOff(), and MCU_DISPLAY::Text.

Referenced by SegmentLCD_LowerHex(), and SegmentLCD_LowerNumber().

Variable Documentation

const uint16_t Blocks[]
static
Initial value:
= {
0x0000,
0x00E0,
0x001F,
0x00FF
}

Defines highlighted segments for the block display.

Definition at line 345 of file segmentlcd.c.

Referenced by displayBlock().

const uint16_t Segment_Numbers[]
static
Initial value:
= {
0x003f,
0x0006,
0x005b,
0x004f,
0x0066,
0x006d,
0x007d,
0x0007,
0x007f,
0x006f,
0x0077,
0x007c,
0x0039,
0x005e,
0x0079,
0x0071,
0x0040
}

Defines higlighted segments for the numeric display.

Definition at line 321 of file segmentlcd.c.

Referenced by SegmentLCD_Number(), and SegmentLCD_UnsignedHex().