ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP
ACMP initialization structure.
Definition at line
733
of file
em_acmp.h
.
#include <
em_acmp.h
>
Field Documentation
| ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy |
ACMP accuracy mode. Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
Definition at line
771
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| uint32_t ACMP_Init_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
Definition at line
748
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::enable |
If true, ACMP is enabled after configuration.
Definition at line
823
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::fullBias |
Full-bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
737
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_0 |
Hysteresis when ACMP output is 0.
Definition at line
791
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_1 |
Hysteresis when ACMP output is 1.
Definition at line
794
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by ACMP during warmup.
Definition at line
804
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange |
Input range. Adjust this setting to optimize the performance for a given input voltage range.
Definition at line
763
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::interruptOnFallingEdge |
Enable setting the interrupt flag on the falling edge.
Definition at line
752
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| bool ACMP_Init_TypeDef::interruptOnRisingEdge |
Enable setting the interrupt flag on the rising edge.
Definition at line
756
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| ACMP_PowerSource_TypeDef ACMP_Init_TypeDef::powerSource |
Select the power source for the ACMP.
Definition at line
776
of file
em_acmp.h
.
Referenced by ACMP_Init() .
| ACMP_VLPInput_Typedef ACMP_Init_TypeDef::vlpInput |
VLP Input source. Select between using VADIV or VBDIV as the VLP source.
Definition at line
800
of file
em_acmp.h
.
Referenced by ACMP_Init() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_acmp.h