LESENSE_CoreCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
Core control (LESENSE_CTRL) descriptor structure.
Definition at line
488
of file
em_lesense.h
.
#include <
em_lesense.h
>
Field Documentation
| LESENSE_BiasMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::biasMode |
| bool LESENSE_CoreCtrlDesc_TypeDef::bufOverWr |
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
Definition at line
513
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_BufTrigLevel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel |
Select trigger conditions for the interrupt and DMA.
Definition at line
516
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::debugRun |
Set to true to keep LESENSE running in the debug mode.
Definition at line
525
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::dualSample |
Set to true to sample both ACMPs simultaneously.
Definition at line
505
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP0 |
Set to true to invert ACMP0 output.
Definition at line
499
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP1 |
Set to true to invert ACMP1 output.
Definition at line
502
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::prsSel |
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
Definition at line
493
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_ScanConfSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanConfSel |
Select scan configuration register usage strategy.
Definition at line
496
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_ScanMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanStart |
Select scan start mode to control how the scan start is being triggered.
Definition at line
490
of file
em_lesense.h
.
Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::storeScanRes |
Set to true in order to store SCANRES in the RAM (accessible via RESDATA) after each scan.
Definition at line
509
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_DMAWakeUp_TypeDef LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA |
Configure trigger condition for the DMA wakeup from EM2.
Definition at line
519
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_lesense.h