MSDSCSI_Inquiry_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD
SCSI Inquiry Command Descriptor Block (CDB) typedef.
Definition at line
58
of file
msdscsi.h
.
#include <
msdscsi.h
>
Data Fields |
|
| struct { | |
| uint8_t Evpd : 1 | |
| uint8_t Obsolete : 1 | |
| uint8_t Reserved : 6 | |
| }; | |
| uint16_t | AllocationLength |
| uint8_t | Control |
| uint8_t | OpCode |
| uint8_t | PageCode |
Field Documentation
| uint16_t MSDSCSI_Inquiry_TypeDef::AllocationLength |
Number of inquiry data bytes requested.
Definition at line
66
of file
msdscsi.h
.
| uint8_t MSDSCSI_Inquiry_TypeDef::Control |
Control byte.
Definition at line
67
of file
msdscsi.h
.
| uint8_t MSDSCSI_Inquiry_TypeDef::Evpd |
Enable Vital Product data.
Definition at line
61
of file
msdscsi.h
.
| uint8_t MSDSCSI_Inquiry_TypeDef::Obsolete |
Obsolete, expect any value.
Definition at line
62
of file
msdscsi.h
.
| uint8_t MSDSCSI_Inquiry_TypeDef::OpCode |
Command opcode.
Definition at line
59
of file
msdscsi.h
.
| uint8_t MSDSCSI_Inquiry_TypeDef::PageCode |
Pagecode.
Definition at line
65
of file
msdscsi.h
.
| uint8_t MSDSCSI_Inquiry_TypeDef::Reserved |
Reserved, expect 0.
Definition at line
63
of file
msdscsi.h
.
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/
msdscsi.h