SE_Status_t Struct ReferenceEMLIB > SE
Definition at line
364
of file
em_se.h
.
Data Fields |
|
uint32_t | bootStatus |
SE_DebugStatus_t | debugStatus |
uint32_t | hostFwVersion |
bool | secureBootEnabled |
uint32_t | seFwVersion |
Field Documentation
uint32_t SE_Status_t::bootStatus |
Boot status code / error code (Bits [7:0]).
Definition at line
366
of file
em_se.h
.
Referenced by SE_getStatus() .
SE_DebugStatus_t SE_Status_t::debugStatus |
uint32_t SE_Status_t::hostFwVersion |
Host firmware version (if available).
Definition at line
370
of file
em_se.h
.
Referenced by SE_getStatus() .
bool SE_Status_t::secureBootEnabled |
uint32_t SE_Status_t::seFwVersion |
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_se.h