DPLL initialization structure. Frequency will be Fref*(N+1)/(M+1).
Definition at line 630
of file em_cmu.h
.
#include <
em_cmu.h
>
Data Fields | |
bool | autoRecover |
bool | ditherEn |
CMU_DPLLEdgeSel_TypeDef | edgeSel |
uint32_t | frequency |
CMU_DPLLLockMode_TypeDef | lockMode |
uint16_t | m |
uint16_t | n |
CMU_Select_TypeDef | refClk |
Field Documentation
bool CMU_DPLLInit_TypeDef::autoRecover |
Enable automatic lock recovery.
Definition at line 637
of file em_cmu.h
.
Referenced by CMU_DPLLLock().
bool CMU_DPLLInit_TypeDef::ditherEn |
Enable dither functionalityery.
Definition at line 638
of file em_cmu.h
.
Referenced by CMU_DPLLLock().
CMU_DPLLEdgeSel_TypeDef CMU_DPLLInit_TypeDef::edgeSel |
Reference clock edge detect selector.
Definition at line 635
of file em_cmu.h
.
Referenced by CMU_DPLLLock().
uint32_t CMU_DPLLInit_TypeDef::frequency |
PLL frequency value, max 80 MHz.
Definition at line 631
of file em_cmu.h
.
Referenced by CMU_DPLLLock().
CMU_DPLLLockMode_TypeDef CMU_DPLLInit_TypeDef::lockMode |
uint16_t CMU_DPLLInit_TypeDef::m |
uint16_t CMU_DPLLInit_TypeDef::n |
CMU_Select_TypeDef CMU_DPLLInit_TypeDef::refClk |
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_cmu.h