TEXTDISPLAY_Config_t Struct Reference
Initialization data structure for text display devices.
Definition at line 82
of file textdisplay.h
.
#include <
textdisplay.h
>
Data Fields | |
int | displayDeviceNo |
bool | lfToCrLf |
bool | scrollEnable |
Field Documentation
int TEXTDISPLAY_Config_t::displayDeviceNo |
Display device number to initialize test display on.
Definition at line 83
of file textdisplay.h
.
Referenced by RETARGET_TextDisplayInit(), and TEXTDISPLAY_New().
bool TEXTDISPLAY_Config_t::lfToCrLf |
Enable or disable LF to CR+LF conversion.
Definition at line 90
of file textdisplay.h
.
Referenced by RETARGET_TextDisplayInit(), and TEXTDISPLAY_New().
bool TEXTDISPLAY_Config_t::scrollEnable |
Enable/disable scrolling mode on the text display. Scrolling mode will consume more memory because the lines will have to be stored in memory.
Definition at line 85
of file textdisplay.h
.
Referenced by RETARGET_TextDisplayInit(), and TEXTDISPLAY_New().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/hardware/kit/common/drivers/
textdisplay.h