IADC_Result_t Struct Reference

Structure holding IADC result, including data and ID

Definition at line 813 of file em_iadc.h.

#include <em_iadc.h>

Data Fields

uint32_t data
 
uint8_t id
 

Field Documentation

uint32_t IADC_Result_t::data

ADC sample data.

Definition at line 814 of file em_iadc.h.

uint8_t IADC_Result_t::id

Id of FIFO entry; Scan table entry id or single indicator (0x20).

Definition at line 815 of file em_iadc.h.


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/em_iadc.h