Direct_Transmit_Plugin

Detailed Description

Direct transmit plugin, see Plugin System Layer for detailed documentation.

.

Data Structures

struct  EZRADIODRV_DirectTxHandle
 EzRadio direct tx plug-in instance initialization and handler structure.
 

Macros

#define EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT
 Configuration data for EzRadio direct tx plug-in.
 

Typedefs

typedef struct EZRADIODRV_DirectTxHandle EZRADIODRV_DirectTxHandle_t
 EzRadio direct tx plug-in instance initialization and handler structure.
 

Functions

Ecode_t ezradioStartDirectTransmit (EZRADIODRV_Handle_t radioHandle)
 Starts direct transmission with the radio configurations from the radioHandle parameter.
 
Ecode_t ezradioStopDirectTransmit (void)
 Stops direct transmission.
 

Macro Definition Documentation

#define EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT
Value:
{ /* PN9 */ \
0, /* Channel */ \
},

Configuration data for EzRadio direct tx plug-in.

Definition at line 71 of file ezradio_direct_transmit_plugin.h.

Function Documentation

Ecode_t ezradioStartDirectTransmit ( EZRADIODRV_Handle_t  radioHandle)

Starts direct transmission with the radio configurations from the radioHandle parameter.

Parameters
radioHandleHandler of the EzRadio driver instance where channel configuration is set.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 54 of file ezradio_direct_transmit_plugin.c.

References EZRADIODRV_DirectTxHandle::channel, EZRADIODRV_HandleData::directTx, ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE, ECODE_EMDRV_EZRADIODRV_OK, ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED, ezradio_get_int_status(), ezradio_request_device_state(), and ezradio_start_tx().

Ecode_t ezradioStopDirectTransmit ( void  )

Stops direct transmission.

Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 85 of file ezradio_direct_transmit_plugin.c.

References ECODE_EMDRV_EZRADIODRV_OK, and ezradio_change_state().