TempSensor
Detailed Description
Driver for DS75 I2C temperature sensor.
Data Structures |
|
| struct | TEMPSENS_Temp_TypeDef |
Macros |
|
| #define | TEMPSENS_DK_ADDR 0x90 |
Enumerations |
|
| enum |
TEMPSENS_Register_TypeDef
{
tempsensRegTemp = 0, tempsensRegConfig = 1, tempsensRegHysteresis = 2, tempsensRegShutdown = 3 } |
Functions |
|
| void | TEMPSENS_Celsius2Fahrenheit ( TEMPSENS_Temp_TypeDef *temp) |
|
Convert temperature from Celsius to Fahrenheit.
|
|
| int | TEMPSENS_RegisterGet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Register_TypeDef reg, uint16_t *val) |
|
Read sensor register content.
|
|
| int | TEMPSENS_RegisterSet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Register_TypeDef reg, uint16_t val) |
|
Write to sensor register.
|
|
| int | TEMPSENS_TemperatureGet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Temp_TypeDef *temp) |
|
Fetch current temperature from temperature sensor (in Celsius).
|
|
Macro Definition Documentation
| #define TEMPSENS_DK_ADDR 0x90 |
I2C device address for temperature sensor on EFM32GG/LG/WG DK
Definition at line
55
of file
tempsens.h
.
Enumeration Type Documentation
Function Documentation
| void TEMPSENS_Celsius2Fahrenheit | ( | TEMPSENS_Temp_TypeDef * |
temp
|
) |
Convert temperature from Celsius to Fahrenheit.
- Parameters
-
[in,out] tempReference to structure to holding temperature in Celsius to convert. Upon return, it has been changed to Fahrenheit.
Definition at line
58
of file
tempsens.c
.
References TEMPSENS_Temp_TypeDef::f , and TEMPSENS_Temp_TypeDef::i .
| int TEMPSENS_RegisterGet | ( | I2C_TypeDef * |
i2c,
|
| uint8_t |
addr,
|
||
| TEMPSENS_Register_TypeDef |
reg,
|
||
| uint16_t * |
val
|
||
| ) |
Read sensor register content.
If reading the temperature register, when a measurement is completed inside the sensor device, the new measurement may not be stored. For this reason, the temperature should not be polled with a higher frequency than the measurement conversion time for a given resolution configuration. Please refer to sensor device datasheet.
- Parameters
-
[in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [in] regRegister to read. [out] valReference to place register read.
- Returns
- Returns 0 if register read, <0 if unable to read register.
Definition at line
99
of file
tempsens.c
.
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE_READ , I2CSPM_Transfer() , i2cTransferDone , I2C_TransferSeq_TypeDef::len , and tempsensRegConfig .
Referenced by TEMPSENS_TemperatureGet() .
| int TEMPSENS_RegisterSet | ( | I2C_TypeDef * |
i2c,
|
| uint8_t |
addr,
|
||
| TEMPSENS_Register_TypeDef |
reg,
|
||
| uint16_t |
val
|
||
| ) |
Write to sensor register.
- Parameters
-
[in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [in] regRegister to write (temperature register cannot be written). [in] valValue used when writing to register.
- Returns
- Returns 0 if register written, <0 if unable to write to register.
Definition at line
156
of file
tempsens.c
.
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE , I2CSPM_Transfer() , i2cTransferDone , I2C_TransferSeq_TypeDef::len , tempsensRegConfig , and tempsensRegTemp .
| int TEMPSENS_TemperatureGet | ( | I2C_TypeDef * |
i2c,
|
| uint8_t |
addr,
|
||
| TEMPSENS_Temp_TypeDef * |
temp
|
||
| ) |
Fetch current temperature from temperature sensor (in Celsius).
If reading the temperature, when a measurement is completed inside the sensor device, the new measurement may not be stored. For this reason, the temperature should not be polled with a higher frequency than the measurement conversion time for a given resolution configuration. Please refer to sensor device datasheet.
- Note
- The sensor on the the DK, STDS75, does not seem to have any check on max temperature limit, ie when exceeding specified max 125 C limit, it will keep increasing 9 bit counter to max representable 9 bit value of 127.5 C and then flip over to negative numbers. There is no limit check in this implementation on such issues.
- Parameters
-
[in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [out] tempReference to structure to place temperature (in Celsius).
- Returns
- Returns 0 if temperature read, <0 if unable to read temperature.
Definition at line
223
of file
tempsens.c
.
References TEMPSENS_Temp_TypeDef::f , TEMPSENS_Temp_TypeDef::i , TEMPSENS_RegisterGet() , and tempsensRegTemp .