HidKeyboard
Detailed Description
Implements a USB HID class keyboard.
HIDKBD Implementation
The source code of the HIDKBD implementation resides in kits/common/drivers/hidkbd.c and
hidkbd.h
. This driver implements a basic USB keyboard. Refer to hidkbd examples for STK3700 and DK3750 for examples using this driver.
HIDKBD Device Configuration Options
This section contains a description of the configuration options for the driver. The options are #define's which are expected to be found in the application "usbconfig.h" header file. The values shown below are from the Giant Gecko STK3700 hidbkd example.
// USB interface number. Interfaces are numbered from zero to one less than // the number of concurrent interfaces supported by the configuration. // The interfac numbers must be 0 standalone HID device, for a // composite device which includes a HID interface it must not be in conflict // with other device interfaces. #define HIDKBD_INTERFACE_NO 0 // Endpoint address for HID input reports. #define HIDKBD_INTR_IN_EP_ADDR 0x81 // The bInterval reported with the interrupt IN endpoint descriptor. #define HIDKBD_POLL_RATE 24 // Timer id, see USBTIMER in the USB device stack documentation. // The HID driver use a timer to implement the idle-rate defined in the HID class spec. #define HIDKBD_IDLE_TIMER 0
Data Structures |
|
| struct | HIDKBD_Init_t |
| struct | HIDKBD_KeyReport_t |
Macros |
|
| #define | DEFAULT_IDLE_RATE 500 |
Typedefs |
|
| typedef void(* | HIDKBD_SetReportFunc_t ) (uint8_t report) |
|
Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device.
|
|
Functions |
|
| void | HIDKBD_Init ( HIDKBD_Init_t *init) |
|
Initialize HID Keyboard driver.
|
|
| void | HIDKBD_KeyboardEvent ( HIDKBD_KeyReport_t *report) |
|
Report a keyboard press/release event.
|
|
| int | HIDKBD_SetupCmd (const USB_Setup_TypeDef *setup) |
|
Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.
|
|
| void | HIDKBD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
|
Handle USB state change events, this function must be called each time the USB device state is changed.
|
|
| const char HIDKBD_ReportDescriptor[69] | SL_ATTRIBUTE_ALIGN (4) |
Variables |
|
| const char | HIDKBD_ReportDescriptor [69] |
Macro Definition Documentation
| #define DEFAULT_IDLE_RATE 500 |
Default idle-rate recommended in the USB HID class specification.
Definition at line
85
of file
hidkbd.c
.
Referenced by HIDKBD_StateChangeEvent() .
Typedef Documentation
| typedef void(* HIDKBD_SetReportFunc_t) (uint8_t report) |
Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device.
- Parameters
-
[in] reportOutput report byte.
Bit 0 : State of keyboard NumLock LED.
Bit 1 : State of keyboard CapsLock LED.
Bit 2 : State of keyboard ScrollLock LED.
Definition at line
72
of file
hidkbd.h
.
Function Documentation
| void HIDKBD_Init | ( | HIDKBD_Init_t * |
init
|
) |
Initialize HID Keyboard driver.
- Parameters
-
[in] initPointer to a HIDKBD_Init_t struct with configuration options.
Definition at line
211
of file
hidkbd.c
.
References HIDKBD_Init_t::hidDescriptor , and HIDKBD_Init_t::setReportFunc .
| void HIDKBD_KeyboardEvent | ( | HIDKBD_KeyReport_t * |
report
|
) |
Report a keyboard press/release event.
- Parameters
-
[in] reportPointer to a HIDKBD_KeyReport_t struct with new key pressed information.
Definition at line
226
of file
hidkbd.c
.
| int HIDKBD_SetupCmd | ( | const USB_Setup_TypeDef * |
setup
|
) |
Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.
- Parameters
-
[in] setupPointer to the setup packet received.
- Returns
- USB_STATUS_OK if command accepted, USB_STATUS_REQ_UNHANDLED when command is unknown. In the latter case the USB device stack will handle the request.
Definition at line
253
of file
hidkbd.c
.
References SL_MIN .
| void HIDKBD_StateChangeEvent | ( | USBD_State_TypeDef |
oldState,
|
| USBD_State_TypeDef |
newState
|
||
| ) |
Handle USB state change events, this function must be called each time the USB device state is changed.
- Parameters
-
[in] oldStateThe device state the device has just left. [in] newStateThe new device state.
Definition at line
350
of file
hidkbd.c
.
References DEFAULT_IDLE_RATE .
| const char HIDKBD_ReportDescriptor [69] SL_ATTRIBUTE_ALIGN | ( | 4 |
|
) |
HID report descriptor created with usb.org's "HID Descriptor Tool(DT)" version 2.4. The descriptor defines an input report which matches the HIDKBD_KeyReport_t typedef, and an output report with 3 bits for controlling NumLock, CapsLock and ScrollLock keyboard LED's