API for STKs and WSTKs

Data Structures

struct BCP_Packet
BCP Packet Structure - Board controller communication protocol version 2.
struct BCP_Packet_
BCP Packet Structure - Board controller communication protocol version 1.
struct BCP_PacketHeader
BCP Packet Header definition.

Macros

#define BSP_BCP_ACK 5
#define BSP_BCP_CURRENT_REPLY 16
#define BSP_BCP_CURRENT_REQ 14
#define BSP_BCP_ECHO_REPLY 11
#define BSP_BCP_ECHO_REQ 10
#define BSP_BCP_ENERGYMODE 22
#define BSP_BCP_FIRST 1
#define BSP_BCP_INVALID 0
#define BSP_BCP_LAST 100
#define BSP_BCP_MAGIC 0xF1
#define BSP_BCP_NET_REPLY 65
#define BSP_BCP_NET_REQUEST 64
#define BSP_BCP_PACKET_SIZe 30
#define BSP_BCP_PACKET_SIZE 132
#define BSP_BCP_STDERR 26
#define BSP_BCP_STDOUT 24
#define BSP_BCP_TEST 32
#define BSP_BCP_TEST_REPLY 33
#define BSP_BCP_VOLTAGE_REPLY 20
#define BSP_BCP_VOLTAGE_REQ 18

Enumerations

enum BSP_Peripheral_TypeDef {
BSP_RS232_SHUTDOWN ,
BSP_RS232_UART ,
BSP_RS232_LEUART ,
BSP_I2C ,
BSP_ETH ,
BSP_I2S ,
BSP_TRACE ,
BSP_TOUCH ,
BSP_AUDIO_IN ,
BSP_AUDIO_OUT ,
BSP_ANALOG_DIFF ,
BSP_ANALOG_SE ,
BSP_MICROSD ,
BSP_TFT ,
BSP_IOEXP_LEDS ,
BSP_IOEXP_SENSORS ,
BSP_IOEXP_DISPLAY ,
BSP_IOEXP_VCOM ,
BSP_VCOM
}

Functions

int BSP_BccDeInit (void)
Deinitialize board controller communication support (BCC) functionality. Reverse actions performed by BSP_BccInit() .
int BSP_BccInit (void)
Initialize board controller communication support (BCC) functionality.
bool BSP_BccPacketReceive ( BCP_Packet *pkt)
Get a packet from the board controller.
int BSP_BccPacketSend ( BCP_Packet *pkt)
Send a packet to the board controller.
void BSP_BccPinsEnable (bool enable)
Enable GPIO pins for the USART/LEUART used for board communication.
float BSP_CurrentGet (void)
Request AEM (Advanced Energy Monitoring) current from board controller.
int BSP_EbiDeInit (void)
Deinitialize the EBI interface for accessing the onboard nandflash.
int BSP_EbiInit (void)
Initialize the EBI interface for accessing the onboard nandflash.
uint32_t BSP_IOExpGetDeviceId (void)
Get IO Expander Device id.
float BSP_VoltageGet (void)
Request AEM (Advanced Energy Monitoring) voltage from board controller.

Macro Definition Documentation

#define BSP_BCP_ACK   5

Generic ACK for one way packages

Definition at line 59 of file bsp_bcp.h .

#define BSP_BCP_CURRENT_REPLY   16

BC Response AEM current

Definition at line 63 of file bsp_bcp.h .

Referenced by BSP_CurrentGet() .

#define BSP_BCP_CURRENT_REQ   14

EFM32 Request AEM current

Definition at line 62 of file bsp_bcp.h .

Referenced by BSP_CurrentGet() .

#define BSP_BCP_ECHO_REPLY   11

BC alive response

Definition at line 61 of file bsp_bcp.h .

#define BSP_BCP_ECHO_REQ   10

EFM32 BC alive request

Definition at line 60 of file bsp_bcp.h .

#define BSP_BCP_ENERGYMODE   22

EFM32 Report Energy Mode (for AEM)

Definition at line 66 of file bsp_bcp.h .

#define BSP_BCP_FIRST   1

Smallest numerical value of message type

Definition at line 57 of file bsp_bcp.h .

Referenced by BSP_BccPacketReceive() .

#define BSP_BCP_INVALID   0

Invalid packet received

Definition at line 55 of file bsp_bcp.h .

#define BSP_BCP_LAST   100

Last defined message type

Definition at line 74 of file bsp_bcp.h .

Referenced by BSP_BccPacketReceive() .

#define BSP_BCP_MAGIC   0xF1

Magic byte to indicate start of packet

Definition at line 76 of file bsp_bcp.h .

Referenced by BSP_BccPacketReceive() , and BSP_BccPacketSend() .

#define BSP_BCP_NET_REPLY   65

Net gateway reply packet

Definition at line 72 of file bsp_bcp.h .

#define BSP_BCP_NET_REQUEST   64

Net gateway request packet

Definition at line 71 of file bsp_bcp.h .

#define BSP_BCP_PACKET_SIZe   30

Max packet size for version 1 of the protocol.

Definition at line 82 of file bsp_bcp.h .

#define BSP_BCP_PACKET_SIZE   132

Max packet size for version 2 of the protocol.

Definition at line 102 of file bsp_bcp.h .

Referenced by BSP_BccPacketReceive() .

#define BSP_BCP_STDERR   26

Debug packet (not used)

Definition at line 68 of file bsp_bcp.h .

#define BSP_BCP_STDOUT   24

Debug packet (not used)

Definition at line 67 of file bsp_bcp.h .

#define BSP_BCP_TEST   32

Reserved type for test

Definition at line 69 of file bsp_bcp.h .

#define BSP_BCP_TEST_REPLY   33

Reserved type for test (reply)

Definition at line 70 of file bsp_bcp.h .

#define BSP_BCP_VOLTAGE_REPLY   20

BC Response AEM voltage

Definition at line 65 of file bsp_bcp.h .

Referenced by BSP_VoltageGet() .

#define BSP_BCP_VOLTAGE_REQ   18

EFM32 Request AEM voltage

Definition at line 64 of file bsp_bcp.h .

Referenced by BSP_VoltageGet() .

Enumeration Type Documentation

Peripherals control structure for STK's, WSTK's and similar.

Enumerator
BSP_RS232_SHUTDOWN

Disable RS232

BSP_RS232_UART

UART control of RS232

BSP_RS232_LEUART

LEUART control of RS232

BSP_I2C

I2C interface

BSP_ETH

Ethernet

BSP_I2S

Audio I2S

BSP_TRACE

ETM Trace

BSP_TOUCH

Display touch interface

BSP_AUDIO_IN

Audio In

BSP_AUDIO_OUT

Audio Out

BSP_ANALOG_DIFF

Differential analog input

BSP_ANALOG_SE

Single ended analog input

BSP_MICROSD

MicroSD SPI interace

BSP_TFT

SSD2119 TFT controller

BSP_IOEXP_LEDS

I/O expander LED control

BSP_IOEXP_SENSORS

I/O expander Humidity & temperature sensor control

BSP_IOEXP_DISPLAY

I/O expander Memory LCD control

BSP_IOEXP_VCOM

I/O expander VCOM (virtual com port) control

BSP_VCOM

VCOM (virtual com port) control

Definition at line 160 of file bsp.h .

Function Documentation

int BSP_BccDeInit ( void )

Deinitialize board controller communication support (BCC) functionality. Reverse actions performed by BSP_BccInit() .

Returns
BSP_STATUS_OK .

Definition at line 74 of file bsp_bcc.c .

References BSP_BccPinsEnable() , BSP_STATUS_OK , CMU_ClockEnable() , LEUART_Reset() , and USART_Reset() .

int BSP_BccInit ( void )
bool BSP_BccPacketReceive ( BCP_Packet * pkt )

Get a packet from the board controller.

Parameters
[in] pkt Pointer to a BCP_Packet instance.
Returns
True if packet received without errors, false otherwise.

Definition at line 152 of file bsp_bcc.c .

References BSP_BCP_FIRST , BSP_BCP_LAST , BSP_BCP_MAGIC , BSP_BCP_PACKET_SIZE , BCP_Packet::magic , BCP_Packet::payloadLength , and BCP_Packet::type .

Referenced by BSP_CurrentGet() , and BSP_VoltageGet() .

int BSP_BccPacketSend ( BCP_Packet * pkt )

Send a packet to the board controller.

Parameters
[in] pkt Pointer to a BCP_Packet instance.
Returns
BSP_STATUS_OK .

Definition at line 205 of file bsp_bcc.c .

References BSP_BCP_MAGIC , BSP_STATUS_OK , BCP_Packet::data , BCP_Packet::magic , BCP_Packet::payloadLength , BCP_Packet::reserved , and BCP_Packet::type .

Referenced by BSP_CurrentGet() , and BSP_VoltageGet() .

void BSP_BccPinsEnable ( bool enable )

Enable GPIO pins for the USART/LEUART used for board communication.

Parameters
[in] enable Set to true to enable pins, set to false to disable.

Definition at line 239 of file bsp_bcc.c .

References GPIO_PinModeSet() , gpioModeDisabled , gpioModeInput , and gpioModePushPull .

Referenced by BSP_BccDeInit() , and BSP_BccInit() .

float BSP_CurrentGet ( void )

Request AEM (Advanced Energy Monitoring) current from board controller.

Note
Assumes that BSP_Init() has been called with BSP_INIT_BCC bitmask.
Returns
The current expressed in milliamperes. Returns 0.0 on board controller communication error.

Definition at line 357 of file bsp_stk.c .

References BSP_BccPacketReceive() , BSP_BccPacketSend() , BSP_BCP_CURRENT_REPLY , BSP_BCP_CURRENT_REQ , BCP_Packet::data , BCP_Packet::payloadLength , and BCP_Packet::type .

int BSP_EbiDeInit ( void )

Deinitialize the EBI interface for accessing the onboard nandflash.

Note
This function is not relevant for Gxxx_STK's. This function is provided for API completeness, it does not perform an actual EBI deinitialization.
Returns
BSP_STATUS_OK or BSP_STATUS_NOT_IMPLEMENTED

Definition at line 178 of file bsp_stk.c .

References BSP_STATUS_NOT_IMPLEMENTED , and BSP_STATUS_OK .

int BSP_EbiInit ( void )

Initialize the EBI interface for accessing the onboard nandflash.

Note
This function is not relevant for Gxxx_STK's.
Returns
BSP_STATUS_OK or BSP_STATUS_NOT_IMPLEMENTED

Definition at line 85 of file bsp_stk.c .

References BSP_STATUS_NOT_IMPLEMENTED , BSP_STATUS_OK , CMU_ClockEnable() , cmuClock_GPIO , cmuClock_HFPER , GPIO_PinModeSet() , gpioModeInput , and gpioModePushPull .

uint32_t BSP_IOExpGetDeviceId ( void )

Get IO Expander Device id.

Returns
The device id of a connected IO Expander Device id or 0 if no IO expander is connected.

Definition at line 194 of file bsp_stk.c .

float BSP_VoltageGet ( void )

Request AEM (Advanced Energy Monitoring) voltage from board controller.

Note
Assumes that BSP_Init() has been called with BSP_INIT_BCC bitmask.
Returns
The voltage. Returns 0.0 on board controller communication error.

Definition at line 392 of file bsp_stk.c .

References BSP_BccPacketReceive() , BSP_BccPacketSend() , BSP_BCP_VOLTAGE_REPLY , BSP_BCP_VOLTAGE_REQ , BCP_Packet::data , BCP_Packet::payloadLength , and BCP_Packet::type .