Modules
Here is a list of all modules:
BSP | Board Support Package |
API for DKs | |
API for STKs and WSTKs | |
Common BSP for all kits | |
Device Initialization | Device Initialization using HAL configuration |
Thunderboard Sense BSP | BSP for Thunderboard Sense and Thunderboard Sense 2 |
BAP - Barometric Pressure Sensor | Driver for the Bosch Sensortec BMP280 pressure sensor |
BOARD Module for Thunderboard Sense | Board hardware control, configuraton and miscellaneous functions |
Power and Interrupt Controller Definitions | Thunderboard Sense 1 Power and Interrupt Controller register and bitfield definitions |
BOARD Module for Thunderboard Sense 2 | Board hardware control, configuraton and miscellaneous functions |
CCS811 - Indoor Air Quality Sensor | Driver for the Cambridge CMOS Sensors CCS811 gas and indoor air quality sensor |
HALL - Hall Effect Sensor | Driver for Hall effect sensor |
Si7210 - Hall Effect Sensor | Driver for the Silicon Labs Si7210 Hall effect sensor |
ICM20648 - 6-axis Motion Sensor Driver | Driver for the Invensense ICM20648 6-axis motion sensor |
IMU - Inertial Measurement Unit | Inertial Measurement Unit driver |
MIC - Microphone Driver (ADC) | Driver for the Knowles SPV1840LR5H-B MEMS Microphone |
MIC - Microphone Driver (I2S) | Driver for the Invensense ICS-43434 MEMS Microphone |
SI1133 - Ambient Light and UV Index Sensor | Driver for the Silicon Labs Si1133 Ambient Light and UV sensor |
SI7021 - Relative Humidity and Temperature Sensor | Driver for the Silicon Labs Si7021 I2C Humidity and Temperature Sensor |
Utility Functions | Utility functions |
Devices | Silicon Laboratories CMSIS-CORE device system headers |
EFR32 | |
EMDRV | Gecko Platform driver library |
DMADRV | DMADRV Direct Memory Access Driver |
EZRADIODRV | EZR32 EzRadio Peripheral Interface Driver |
API_Layer | EzRadio API Layer |
COMM_Layer | EzRadio Communication Layer |
HAL_Layer | EzRadio HAL Layer |
Plugin_System | EzRadio Plugin System Layer, see Plugin System Layer for detailed documentation. |
Auto_ACK_Plugin | Auto acknowledge plugin, see Plugin System Layer for detailed documentation. |
CRC_Error_Plugin | CRC error plugin, see Plugin System Layer for detailed documentation. |
Direct_Receive_Plugin | Direct receive plugin, see Plugin System Layer for detailed documentation. |
Direct_Transmit_Plugin | Direct transmit plugin, see Plugin System Layer for detailed documentation. |
PN9_Plugin | Pseudo random transmit plugin, see Plugin System Layer for detailed documentation. |
Plugin_Manager | Plugin manager, see Plugin System Layer for detailed documentation. |
Receive_Plugin | Receive plugin, see Plugin System Layer for detailed documentation. |
Transmit_Plugin | Transmit plugin, see Plugin System Layer for detailed documentation. |
Unmod_Carrier_Plugin | Unmodulated Carrier plugin, see Plugin System Layer for detailed documentation. |
GPIOINT | GPIOINT General Purpose Input/Output Interrupt dispatcher |
NVM | NVM Non-volatile Memory Wear-Leveling Driver |
NVM3 | NVM3 Non-Volatile Memory Management driver |
NVM3Hal | NVM3 HAL module |
NVM3Lock | NVM3 lock module |
RTCDRV | Real-time Clock Driver |
SLEEP | Sleep Management Driver |
SPIDRV | SPIDRV Serial Peripheral Interface Driver |
TEMPDRV | TEMPDRV Temperature Sensor Driver |
UARTDRV | UARTDRV Universal Asynchronous Receiver/Transmitter Driver |
USTIMER | USTIMER Microsecond Delay Timer Driver |
EMLIB | Low-level peripheral library |
ACMP | Analog comparator (ACMP) Peripheral API |
ADC | Analog to Digital Converter (ADC) Peripheral API |
ASSERT | Error checking module |
BUS | BUS register and RAM bit/field read/write API |
CHIP | Chip errata workarounds initialization API |
CMU | Clock management unit (CMU) Peripheral API |
COMMON | General purpose utilities and cross-compiler support |
CORE | Core interrupt handling API |
CRYOTIMER | Ultra Low Energy Timer/Counter (CRYOTIMER) Peripheral API |
CRYPTO | Cryptography accelerator peripheral API |
DBG | Debug (DBG) Peripheral API |
EMU | Energy Management Unit (EMU) Peripheral API |
GPCRC | General Purpose Cyclic Redundancy Check (GPCRC) API |
GPIO | General Purpose Input/Output (GPIO) API |
I2C | Inter-integrated Circuit (I2C) Peripheral API |
IDAC | Current Digital-to-Analog Converter (IDAC) Peripheral API |
INT | Safe nesting of interrupt disable/enable API |
LDMA | Linked Direct Memory Access (LDMA) Peripheral API |
LETIMER | Low Energy Timer (LETIMER) Peripheral API |
LEUART | Low Energy Universal Asynchronous Receiver/Transmitter (LEUART) Peripheral API |
MPU | Memory Protection Unit (MPU) Peripheral API |
MSC | Memory System Controller API |
PCNT | Pulse Counter (PCNT) Peripheral API |
PRS | Peripheral Reflex System (PRS) Peripheral API |
RAMFUNC | RAM code support |
RMU | Reset Management Unit (RMU) Peripheral API |
RTCC | Real Time Counter (RTCC) Peripheral API |
SYSTEM | System API |
TIMER | Timer/Counter (TIMER) Peripheral API |
USART | Universal Synchronous/Asynchronous Receiver/Transmitter Peripheral API |
VERSION | Version API |
WDOG | Watchdog (WDOG) Peripheral API |
External Device Drivers | External Device Drivers is a collection of device drivers for external components. These components are typically Silicon Laboratories ICs that are not part of the Gecko families of SoCs |
EFP Driver | EFP (Energy Friendly PMIC) driver |
Kit Drivers | Kit support and drivers |
CPT112S_I2C | Silicon Labs 12-pad Capacitive Touch Evaluation Board I2C driver |
CapSense | Capacitive sensing driver |
Display | Display device driver stack library |
DmaCtrl | UDMA control block array |
EEPROM | I2C EEPROM Driver |
Gecko USB MSD | USB Mass Storage Class (MSC) |
Gecko USB RS232 bridge | Gecko USB to RS232 bridge (CDC Class) |
HidKeyboard | Implements a USB HID class keyboard |
I2CSPM | I2C Simple Polled Master driver |
Ksz8851snl | KSZ8851SNL SPI Ethernet Controller driver |
MicroSd | SPI driver for micro SD card |
NANDFlash | Driver for Numonyx NAND256W3A NAND Flash devices |
NORFlash | Driver for Spanion S29GL128P90FFIR13 and S29GL064N NOR Flash devices |
RetargetIo | Standard I/O retargeting driver |
SegmentLcd | Segment LCD driver |
Si114x | Silicon Labs Si114x Ultraviolet (UV) Index, Gesture, Proximity, and Ambient Light Sensor I2C driver |
Si7013 | Silicon Labs Si7013 Relative Humidity and Temperature Sensor I2C driver |
Si72xx | Silicon Labs Si72xx Magnetic Hall Effect Sensor I2C driver |
TFT | Driver for SSD2119 TFT in Direct Drive or Adress Mapped mode |
TempSensor | Driver for DS75 I2C temperature sensor |
Textdisplay | Line based text output terminal interface on top of the DISPLAY device driver stack. See TextDisplay Library for more information |
Touch | Touch panel driver for DK3650, DK3750 and DK3850 Development Kits |
Udelay | Calibrated busy wait loop |
UsbHid | USB HID keyboard scan codes |
VddCheck | VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API |
Platform Common | Gecko Platform Common components are used throughout the Gecko SDK |
BIT | |
SLIST | |
Status Codes | |
Platform Middleware | Gecko Platform Middleware for use with EFM32, EZR32 and EFR32 products |
Capacitive Sensing Firmware Library | Capacitive sensing firmware library for Silicon Labs MCUs |
GLIB | Graphics Library |
Platform Services | Gecko Platform Service components are high-level, device-independent and thread-safe APIs. Each service may have a hardware abstraction layer (HAL) |
MPU | MPU basic utilities |
SLEEPTIMER | Low frequency timer utilities. Utilities (timer, delays and time keeping) |