CMU_HFXOInit_TypeDef Struct Reference

HFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.

Definition at line 2413 of file em_cmu.h.

#include <em_cmu.h>

Data Fields

bool autoSelEm01
 
bool autoStartEm01
 
bool autoStartSelOnRacWakeup
 
uint16_t ctuneStartup
 
uint16_t ctuneSteadyState
 
bool lowPowerMode
 
CMU_OscMode_TypeDef mode
 
uint8_t regIshSteadyState
 
uint8_t thresholdPeakDetect
 
uint8_t timeoutPeakDetect
 
uint8_t timeoutShuntOptimization
 
uint8_t timeoutStartup
 
uint8_t timeoutSteady
 
uint8_t xoCoreBiasTrimStartup
 
uint8_t xoCoreBiasTrimSteadyState
 

Field Documentation

bool CMU_HFXOInit_TypeDef::autoSelEm01
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 2425 of file em_cmu.h.

Referenced by CMU_HFXOInit().

bool CMU_HFXOInit_TypeDef::autoStartEm01
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 2424 of file em_cmu.h.

Referenced by CMU_HFXOInit().

bool CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 2426 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint16_t CMU_HFXOInit_TypeDef::ctuneStartup

Startup phase CTUNE (load capacitance) value

Definition at line 2427 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState

Steady-state phase CTUNE (load capacitance) value

Definition at line 2428 of file em_cmu.h.

Referenced by BSP_initClocks(), and CMU_HFXOInit().

bool CMU_HFXOInit_TypeDef::lowPowerMode

Enable low-power mode

Definition at line 2423 of file em_cmu.h.

Referenced by CMU_HFXOInit().

CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode

Oscillator mode

Definition at line 2442 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::regIshSteadyState

Shunt steady-state current

Definition at line 2429 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::thresholdPeakDetect

Peak detection threshold

Definition at line 2432 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect

Timeout - peak detection

Definition at line 2434 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::timeoutShuntOptimization

Timeout - shunt optimization

Definition at line 2433 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::timeoutStartup

Timeout - startup

Definition at line 2436 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::timeoutSteady

Timeout - steady-state

Definition at line 2435 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup

Startup XO core bias current trim

Definition at line 2430 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState

Steady-state XO core bias current trim

Definition at line 2431 of file em_cmu.h.

Referenced by CMU_HFXOInit().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/em_cmu.h