CMU_LFXOInit_TypeDef Struct Reference

LFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.

Definition at line 2367 of file em_cmu.h.

#include <em_cmu.h>

Data Fields

uint8_t ctune
 
uint8_t gain
 
CMU_OscMode_TypeDef mode
 
uint8_t timeout
 

Field Documentation

uint8_t CMU_LFXOInit_TypeDef::ctune

CTUNE (load capacitance) value

Definition at line 2369 of file em_cmu.h.

Referenced by BSP_initClocks(), and CMU_LFXOInit().

uint8_t CMU_LFXOInit_TypeDef::gain

Gain/max startup margin

Definition at line 2370 of file em_cmu.h.

Referenced by CMU_LFXOInit().

CMU_OscMode_TypeDef CMU_LFXOInit_TypeDef::mode

Oscillator mode

Definition at line 2375 of file em_cmu.h.

Referenced by CMU_LFXOInit().

uint8_t CMU_LFXOInit_TypeDef::timeout

Startup delay

Definition at line 2374 of file em_cmu.h.

Referenced by CMU_LFXOInit().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/em_cmu.h