TOUCH_Pos_TypeDef Struct Reference

Touch panel position structure

Definition at line 60 of file touch.h.

#include <touch.h>

Data Fields

uint16_t adcx
 
uint16_t adcy
 
uint8_t pen
 
uint16_t x
 
uint16_t y
 

Field Documentation

uint16_t TOUCH_Pos_TypeDef::adcx

ADC X readings

Definition at line 63 of file touch.h.

Referenced by ADC0_IRQHandler(), TOUCH_GetPos(), and TOUCH_RecalculatePosition().

uint16_t TOUCH_Pos_TypeDef::adcy

ADC Y readings

Definition at line 64 of file touch.h.

Referenced by ADC0_IRQHandler(), TOUCH_GetPos(), and TOUCH_RecalculatePosition().

uint8_t TOUCH_Pos_TypeDef::pen

0=not pressed, 1=touched

Definition at line 65 of file touch.h.

Referenced by ADC0_IRQHandler(), TOUCH_GetPos(), TOUCH_RecalculatePosition(), and TOUCH_StateChanged().

uint16_t TOUCH_Pos_TypeDef::x

x position

Definition at line 61 of file touch.h.

Referenced by ADC0_IRQHandler(), TOUCH_GetPos(), TOUCH_RecalculatePosition(), and TOUCH_StateChanged().

uint16_t TOUCH_Pos_TypeDef::y

y position

Definition at line 62 of file touch.h.

Referenced by ADC0_IRQHandler(), TOUCH_GetPos(), TOUCH_RecalculatePosition(), and TOUCH_StateChanged().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/hardware/kit/common/drivers/touch.h