sl_mpu.c File Reference

MPU API implementation.

Version
1.0.0

License

(C) Copyright 2018 Silicon Labs, www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file sl_mpu.c .

#include "em_device.h"
#include " em_common.h "
#include " em_core.h "
#include " sl_mpu.h "
#include <stdlib.h>
#include <math.h>

Macros

#define MPU_RAM_BACKGROUND_XN_REGION_NBR 0u
#define MPU_RAM_FUNCTION_REGION_NBR 1u
#define MPU_RBAR_VALUE ARM_MPU_RBAR(0u, ARM_MPU_SH_OUTER, 0, 1, 1)
#define MPU_SUBREGION_NBR 8u
#define MPU_SUBREGION_USE_MIN_SIZE 256u
#define RAMFUNC_SECTION_BEGIN (uint32_t) &__ram_func_section_start
#define RAMFUNC_SECTION_END (uint32_t) &__ram_func_section_end
#define RAMFUNC_SECTION_SIZE (RAMFUNC_SECTION_END - RAMFUNC_SECTION_BEGIN)

Functions

void MemManage_Handler (void)
static void mpu_compute_region_data (uint32_t section_begin, uint32_t section_end, uint32_t section_size, uint32_t *mpu_region_begin, uint32_t *mpu_region_end, uint32_t *mpu_region_size)
__WEAK void mpu_fault_handler (void)
static uint8_t mpu_region_size_encode (uint32_t region_size)
static uint32_t mpu_round_up_next_pwr2 (uint32_t nbr)
void sl_mpu_disable_execute (uint32_t address_begin, uint32_t address_end, uint32_t size)
void sl_mpu_disable_execute_from_ram (void)

Variables

uint32_t __ram_func_section_end
uint32_t __ram_func_section_start
static uint32_t region_nbr = 0

Function Documentation

static void mpu_compute_region_data ( uint32_t section_begin,
uint32_t section_end,
uint32_t section_size,
uint32_t * mpu_region_begin,
uint32_t * mpu_region_end,
uint32_t * mpu_region_size
)
static

Compute region size.

Parameters
section_begin Section begin address.
section_end Section end address.
section_size Size of section.
mpu_region_begin Pointer to a region begin variable.
mpu_region_end Pointer to a region end variable.
mpu_region_size Pointer to a region size variable.

Definition at line 299 of file sl_mpu.c .

References mpu_round_up_next_pwr2() .

Referenced by sl_mpu_disable_execute() , and sl_mpu_disable_execute_from_ram() .

__WEAK void mpu_fault_handler ( void )

MemManage default exception handler. Reset target.

Definition at line 333 of file sl_mpu.c .

Referenced by MemManage_Handler() .

static uint8_t mpu_region_size_encode ( uint32_t region_size )
static

Encode region size in RASR register REGION size field format.

Parameters
region_size Size of region.

Definition at line 277 of file sl_mpu.c .

Referenced by sl_mpu_disable_execute() , and sl_mpu_disable_execute_from_ram() .

static uint32_t mpu_round_up_next_pwr2 ( uint32_t nbr )
static

Rounds up given number to next power of 2.

Parameters
nbr Number to round-up to next power of 2.

Definition at line 257 of file sl_mpu.c .

Referenced by mpu_compute_region_data() .