BCP_Packet Struct Reference
BCP Packet Structure - Board controller communication protocol version 2.
Definition at line
105
of file
bsp_bcp.h
.
#include <
bsp_bcp.h
>
Data Fields |
|
| uint8_t | data [ BSP_BCP_PACKET_SIZE ] |
| uint8_t | magic |
| uint8_t | payloadLength |
| uint8_t | reserved |
| uint8_t | type |
Field Documentation
| uint8_t BCP_Packet::data[ BSP_BCP_PACKET_SIZE ] |
BCP Packet Data payload
Definition at line
110
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketSend() , BSP_CurrentGet() , and BSP_VoltageGet() .
| uint8_t BCP_Packet::magic |
Magic - start of packet - must be BSP_BCP_MAGIC
Definition at line
106
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketReceive() , and BSP_BccPacketSend() .
| uint8_t BCP_Packet::payloadLength |
Length of data segment >=0 and <=BSP_BCP_PACKET_SIZE
Definition at line
108
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketReceive() , BSP_BccPacketSend() , BSP_CurrentGet() , and BSP_VoltageGet() .
| uint8_t BCP_Packet::reserved |
Reserved for future expansion
Definition at line
109
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketSend() .
| uint8_t BCP_Packet::type |
Type - packet type
Definition at line
107
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketReceive() , BSP_BccPacketSend() , BSP_CurrentGet() , and BSP_VoltageGet() .
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/hardware/kit/common/bsp/
bsp_bcp.h