EZRADIODRV_FieldLength Struct Reference

EzRadio transmit field length sturcture. Holds length information on all available fields. Data is got from the generated radio configuration header file.

Definition at line 82 of file ezradio_transmit_plugin.h .

#include < ezradio_transmit_plugin.h >

Data Fields

uint8_t f1
Field 1 length.
uint8_t f2
Field 2 length.
uint8_t f3
Field 3 length.
uint8_t f4
Field 4 length.
uint8_t f5
Field 5 length.

The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emdrv/ezradiodrv/plugins/inc/ ezradio_transmit_plugin.h