SE Command structure to which all commands to the SE must adhere.
Definition at line
330
of file
em_se.h
.
#include <
em_se.h
>
Data Fields |
|
| uint32_t | command |
| SE_DataTransfer_t * | data_in |
| SE_DataTransfer_t * | data_out |
| size_t | num_parameters |
| uint32_t | parameters [ SE_MAX_PARAMETERS ] |
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/platform/emlib/inc/
em_se.h