Modules#

otThreadLinkInfo

otMacFilterEntry

otMacCounters

otActiveScanResult

otEnergyScanResult

Link#

This module includes functions that control link-layer configuration.

Enumerations#

enum
OT_MAC_FILTER_ADDRESS_MODE_DISABLED
OT_MAC_FILTER_ADDRESS_MODE_ALLOWLIST
OT_MAC_FILTER_ADDRESS_MODE_DENYLIST
}

Defines address mode of the mac filter.

Typedefs#

typedef struct otThreadLinkInfo

This structure represents link-specific information for messages received from the Thread radio.

typedef uint8_t

Used to iterate through mac filter entries.

Defines address mode of the mac filter.

typedef struct otMacFilterEntry

This structure represents a Mac Filter entry.

typedef struct otMacCounters

This structure represents the MAC layer counters.

typedef struct otActiveScanResult

This structure represents a received IEEE 802.15.4 Beacon.

typedef struct otEnergyScanResult

This structure represents an energy scan result.

typedef void(*
otHandleActiveScanResult)(otActiveScanResult *aResult, void *aContext)

This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.

typedef void(*
otHandleEnergyScanResult)(otEnergyScanResult *aResult, void *aContext)

This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.

typedef void(*
otLinkPcapCallback)(const otRadioFrame *aFrame, bool aIsTx, void *aContext)

This function pointer is called when an IEEE 802.15.4 frame is received.

Functions#

otLinkActiveScan(otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleActiveScanResult aCallback, void *aCallbackContext)

This function starts an IEEE 802.15.4 Active Scan.

bool
otLinkIsActiveScanInProgress(otInstance *aInstance)

This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.

otLinkEnergyScan(otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleEnergyScanResult aCallback, void *aCallbackContext)

This function starts an IEEE 802.15.4 Energy Scan.

bool
otLinkIsEnergyScanInProgress(otInstance *aInstance)

This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.

otLinkSendDataRequest(otInstance *aInstance)

This function enqueues an IEEE 802.15.4 Data Request message for transmission.

bool
otLinkIsInTransmitState(otInstance *aInstance)

This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.

uint8_t
otLinkGetChannel(otInstance *aInstance)

Get the IEEE 802.15.4 channel.

otLinkSetChannel(otInstance *aInstance, uint8_t aChannel)

Set the IEEE 802.15.4 channel.

uint32_t
otLinkGetSupportedChannelMask(otInstance *aInstance)

Get the supported channel mask of MAC layer.

otLinkSetSupportedChannelMask(otInstance *aInstance, uint32_t aChannelMask)

Set the supported channel mask of MAC layer.

const otExtAddress *
otLinkGetExtendedAddress(otInstance *aInstance)

Gets the IEEE 802.15.4 Extended Address.

otLinkSetExtendedAddress(otInstance *aInstance, const otExtAddress *aExtAddress)

Sets the IEEE 802.15.4 Extended Address.

void
otLinkGetFactoryAssignedIeeeEui64(otInstance *aInstance, otExtAddress *aEui64)

Get the factory-assigned IEEE EUI-64.

otLinkGetPanId(otInstance *aInstance)

Get the IEEE 802.15.4 PAN ID.

otLinkSetPanId(otInstance *aInstance, otPanId aPanId)

Set the IEEE 802.15.4 PAN ID.

uint32_t
otLinkGetPollPeriod(otInstance *aInstance)

Get the data poll period of sleepy end device.

otLinkSetPollPeriod(otInstance *aInstance, uint32_t aPollPeriod)

Set/clear user-specified/external data poll period for sleepy end device.

otLinkGetShortAddress(otInstance *aInstance)

Get the IEEE 802.15.4 Short Address.

uint8_t
otLinkGetMaxFrameRetriesDirect(otInstance *aInstance)

This method returns the maximum number of frame retries during direct transmission.

void
otLinkSetMaxFrameRetriesDirect(otInstance *aInstance, uint8_t aMaxFrameRetriesDirect)

This method sets the maximum number of frame retries during direct transmission.

uint8_t
otLinkGetMaxFrameRetriesIndirect(otInstance *aInstance)

This method returns the maximum number of frame retries during indirect transmission.

void
otLinkSetMaxFrameRetriesIndirect(otInstance *aInstance, uint8_t aMaxFrameRetriesIndirect)

This method sets the maximum number of frame retries during indirect transmission.

otLinkFilterGetAddressMode(otInstance *aInstance)

This function gets the address mode of MAC filter.

void
otLinkFilterSetAddressMode(otInstance *aInstance, otMacFilterAddressMode aMode)

This function sets the address mode of MAC filter.

otLinkFilterAddAddress(otInstance *aInstance, const otExtAddress *aExtAddress)

This method adds an Extended Address to MAC filter.

void
otLinkFilterRemoveAddress(otInstance *aInstance, const otExtAddress *aExtAddress)

This method removes an Extended Address from MAC filter.

void
otLinkFilterClearAddresses(otInstance *aInstance)

This method clears all the Extended Addresses from MAC filter.

otLinkFilterGetNextAddress(otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry)

This method gets an in-use address filter entry.

otLinkFilterAddRssIn(otInstance *aInstance, const otExtAddress *aExtAddress, int8_t aRss)

This method adds a fixed received signal strength (in dBm) entry for the messages from a given Extended Address in MAC Filter.

void
otLinkFilterRemoveRssIn(otInstance *aInstance, const otExtAddress *aExtAddress)

This method removes a MAC Filter entry for fixed received signal strength setting for a given Extended Address.

void
otLinkFilterSetDefaultRssIn(otInstance *aInstance, int8_t aRss)

This method sets the default received signal strength (in dBm) on MAC Filter.

void
otLinkFilterClearDefaultRssIn(otInstance *aInstance)

This method clears any previously set default received signal strength (in dBm) on MAC Filter.

void
otLinkFilterClearAllRssIn(otInstance *aInstance)

This method clears all the received signal strength entries (including default RSS-in) on MAC Filter.

otLinkFilterGetNextRssIn(otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry)

This method gets an in-use RssIn filter entry.

void
otLinkSetRadioFilterEnabled(otInstance *aInstance, bool aFilterEnabled)

This function enables/disables IEEE 802.15.4 radio filter mode.

bool
otLinkIsRadioFilterEnabled(otInstance *aInstance)

This function indicates whether the IEEE 802.15.4 radio filter is enabled or not.

uint8_t
otLinkConvertRssToLinkQuality(otInstance *aInstance, int8_t aRss)

This method converts received signal strength to link quality.

int8_t
otLinkConvertLinkQualityToRss(otInstance *aInstance, uint8_t aLinkQuality)

This method converts link quality to typical received signal strength.

const uint32_t *
otLinkGetTxDirectRetrySuccessHistogram(otInstance *aInstance, uint8_t *aNumberOfEntries)

This method gets histogram of retries for a single direct packet until success.

const uint32_t *
otLinkGetTxIndirectRetrySuccessHistogram(otInstance *aInstance, uint8_t *aNumberOfEntries)

This method gets histogram of retries for a single indirect packet until success.

void
otLinkResetTxRetrySuccessHistogram(otInstance *aInstance)

This method clears histogram statistics for direct and indirect transmissions.

otLinkGetCounters(otInstance *aInstance)

Get the MAC layer counters.

void
otLinkResetCounters(otInstance *aInstance)

Resets the MAC layer counters.

void
otLinkSetPcapCallback(otInstance *aInstance, otLinkPcapCallback aPcapCallback, void *aCallbackContext)

This function registers a callback to provide received raw IEEE 802.15.4 frames.

bool
otLinkIsPromiscuous(otInstance *aInstance)

This function indicates whether or not promiscuous mode is enabled at the link layer.

otLinkSetPromiscuous(otInstance *aInstance, bool aPromiscuous)

This function enables or disables the link layer promiscuous mode.

uint8_t
otLinkCslGetChannel(otInstance *aInstance)

This function gets the CSL channel.

otLinkCslSetChannel(otInstance *aInstance, uint8_t aChannel)

Sets the CSL channel.

uint16_t
otLinkCslGetPeriod(otInstance *aInstance)

This function gets the CSL period.

otLinkCslSetPeriod(otInstance *aInstance, uint16_t aPeriod)

Sets the CSL period in units of 10 symbols.

uint32_t
otLinkCslGetTimeout(otInstance *aInstance)

This function gets the CSL timeout.

otLinkCslSetTimeout(otInstance *aInstance, uint32_t aTimeout)

Sets the CSL timeout in seconds.

uint16_t
otLinkGetCcaFailureRate(otInstance *aInstance)

This function returns the current CCA (Clear Channel Assessment) failure rate.

otLinkSetEnabled(otInstance *aInstance, bool aEnable)

This function enables or disables the link layer.

bool
otLinkIsEnabled(otInstance *aInstance)

This function indicates whether or not the link layer is enabled.

otLinkSendEmptyData(otInstance *aInstance)

This function instructs the device to send an empty IEEE 802.15.4 data frame.

Macros#

#define
OT_US_PER_TEN_SYMBOLS OT_RADIO_TEN_SYMBOLS_TIME

Time for 10 symbols in units of microseconds.

#define

Used to indicate no fixed received signal strength was set.

#define

Initializer for otMacFilterIterator.

Enumeration Documentation#

otMacFilterAddressMode#

otMacFilterAddressMode

Defines address mode of the mac filter.

Enumerator
OT_MAC_FILTER_ADDRESS_MODE_DISABLED

Address filter is disabled.

OT_MAC_FILTER_ADDRESS_MODE_ALLOWLIST

Allowlist address filter mode is enabled.

OT_MAC_FILTER_ADDRESS_MODE_DENYLIST

Denylist address filter mode is enabled.


Typedef Documentation#

otThreadLinkInfo#

typedef struct otThreadLinkInfo otThreadLinkInfo

This structure represents link-specific information for messages received from the Thread radio.


otMacFilterIterator#

typedef uint8_t otMacFilterIterator

Used to iterate through mac filter entries.


otMacFilterAddressMode#

typedef enum otMacFilterAddressMode otMacFilterAddressMode

Defines address mode of the mac filter.


otMacFilterEntry#

typedef struct otMacFilterEntry otMacFilterEntry

This structure represents a Mac Filter entry.


otMacCounters#

typedef struct otMacCounters otMacCounters

This structure represents the MAC layer counters.


otActiveScanResult#

typedef struct otActiveScanResult otActiveScanResult

This structure represents a received IEEE 802.15.4 Beacon.


otEnergyScanResult#

typedef struct otEnergyScanResult otEnergyScanResult

This structure represents an energy scan result.


otHandleActiveScanResult#

typedef void(* otHandleActiveScanResult) (otActiveScanResult *aResult, void *aContext) )(otActiveScanResult *aResult, void *aContext)

This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.

Parameters
TypeDirectionArgument NameDescription
[in]aResult

A valid pointer to the beacon information or NULL when the active scan completes.

[in]aContext

A pointer to application-specific context.


otHandleEnergyScanResult#

typedef void(* otHandleEnergyScanResult) (otEnergyScanResult *aResult, void *aContext) )(otEnergyScanResult *aResult, void *aContext)

This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.

Parameters
TypeDirectionArgument NameDescription
[in]aResult

A valid pointer to the energy scan result information or NULL when the energy scan completes.

[in]aContext

A pointer to application-specific context.


otLinkPcapCallback#

typedef void(* otLinkPcapCallback) (const otRadioFrame *aFrame, bool aIsTx, void *aContext) )(const otRadioFrame *aFrame, bool aIsTx, void *aContext)

This function pointer is called when an IEEE 802.15.4 frame is received.

Parameters
TypeDirectionArgument NameDescription
[in]aFrame

A pointer to the received IEEE 802.15.4 frame.

[in]aIsTx

Whether this frame is transmitted, not received.

[in]aContext

A pointer to application-specific context.

Note

  • This callback is called after FCS processing and aFrame may not contain the actual FCS that was received.

  • This callback is called before IEEE 802.15.4 security processing.


Function Documentation#

otLinkActiveScan#

otError otLinkActiveScan (otInstance * aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleActiveScanResult aCallback, void * aCallbackContext)

This function starts an IEEE 802.15.4 Active Scan.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aScanChannels

A bit vector indicating which channels to scan (e.g. OT_CHANNEL_11_MASK).

uint16_t[in]aScanDuration

The time in milliseconds to spend scanning each channel.

otHandleActiveScanResult[in]aCallback

A pointer to a function called on receiving a beacon or scan completes.

void *[in]aCallbackContext

A pointer to application-specific context.


otLinkIsActiveScanInProgress#

bool otLinkIsActiveScanInProgress (otInstance * aInstance)

This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • true if an IEEE 802.15.4 Active Scan is in progress, false otherwise.


otLinkEnergyScan#

otError otLinkEnergyScan (otInstance * aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleEnergyScanResult aCallback, void * aCallbackContext)

This function starts an IEEE 802.15.4 Energy Scan.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aScanChannels

A bit vector indicating on which channels to perform energy scan.

uint16_t[in]aScanDuration

The time in milliseconds to spend scanning each channel.

otHandleEnergyScanResult[in]aCallback

A pointer to a function called to pass on scan result on indicate scan completion.

void *[in]aCallbackContext

A pointer to application-specific context.


otLinkIsEnergyScanInProgress#

bool otLinkIsEnergyScanInProgress (otInstance * aInstance)

This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • true if an IEEE 802.15.4 Energy Scan is in progress, false otherwise.


otLinkSendDataRequest#

otError otLinkSendDataRequest (otInstance * aInstance)

This function enqueues an IEEE 802.15.4 Data Request message for transmission.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otLinkIsInTransmitState#

bool otLinkIsInTransmitState (otInstance * aInstance)

This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

MAC module is in the transmit state during CSMA/CA procedure, CCA, Data, Beacon or Data Request frame transmission and receiving an ACK of a transmitted frame. MAC module is not in the transmit state during transmission of an ACK frame or a Beacon Request frame.

Returns

  • true if an IEEE 802.15.4 MAC is in the transmit state, false otherwise.


otLinkGetChannel#

uint8_t otLinkGetChannel (otInstance * aInstance)

Get the IEEE 802.15.4 channel.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The IEEE 802.15.4 channel.

See Also


otLinkSetChannel#

otError otLinkSetChannel (otInstance * aInstance, uint8_t aChannel)

Set the IEEE 802.15.4 channel.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aChannel

The IEEE 802.15.4 channel.

This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.

See Also


otLinkGetSupportedChannelMask#

uint32_t otLinkGetSupportedChannelMask (otInstance * aInstance)

Get the supported channel mask of MAC layer.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The supported channel mask as uint32_t with bit 0 (lsb) mapping to channel 0, bit 1 to channel 1, so on.


otLinkSetSupportedChannelMask#

otError otLinkSetSupportedChannelMask (otInstance * aInstance, uint32_t aChannelMask)

Set the supported channel mask of MAC layer.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aChannelMask

The supported channel mask (bit 0 or lsb mapping to channel 0, and so on).

This function succeeds only when Thread protocols are disabled.


otLinkGetExtendedAddress#

const otExtAddress * otLinkGetExtendedAddress (otInstance * aInstance)

Gets the IEEE 802.15.4 Extended Address.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • A pointer to the IEEE 802.15.4 Extended Address.


otLinkSetExtendedAddress#

otError otLinkSetExtendedAddress (otInstance * aInstance, const otExtAddress * aExtAddress)

Sets the IEEE 802.15.4 Extended Address.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otExtAddress *[in]aExtAddress

A pointer to the IEEE 802.15.4 Extended Address.

Note

  • Only succeeds when Thread protocols are disabled.


otLinkGetFactoryAssignedIeeeEui64#

void otLinkGetFactoryAssignedIeeeEui64 (otInstance * aInstance, otExtAddress * aEui64)

Get the factory-assigned IEEE EUI-64.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to the OpenThread instance.

otExtAddress *[out]aEui64

A pointer to where the factory-assigned IEEE EUI-64 is placed.


otLinkGetPanId#

otPanId otLinkGetPanId (otInstance * aInstance)

Get the IEEE 802.15.4 PAN ID.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The IEEE 802.15.4 PAN ID.

See Also


otLinkSetPanId#

otError otLinkSetPanId (otInstance * aInstance, otPanId aPanId)

Set the IEEE 802.15.4 PAN ID.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otPanId[in]aPanId

The IEEE 802.15.4 PAN ID.

This function succeeds only when Thread protocols are disabled. A successful call to this function also invalidates the Active and Pending Operational Datasets in non-volatile memory.

See Also


otLinkGetPollPeriod#

uint32_t otLinkGetPollPeriod (otInstance * aInstance)

Get the data poll period of sleepy end device.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The data poll period of sleepy end device in milliseconds.

See Also


otLinkSetPollPeriod#

otError otLinkSetPollPeriod (otInstance * aInstance, uint32_t aPollPeriod)

Set/clear user-specified/external data poll period for sleepy end device.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aPollPeriod

data poll period in milliseconds.

Note

  • This function updates only poll period of sleepy end device. To update child timeout the function otThreadSetChildTimeout() shall be called.

  • Minimal non-zero value should be OPENTHREAD_CONFIG_MAC_MINIMUM_POLL_PERIOD (10ms). Or zero to clear user-specified poll period.

  • User-specified value should be no more than the maximal value 0x3FFFFFF ((1 << 26) - 1) allowed, otherwise it would be clipped by the maximal value.

See Also


otLinkGetShortAddress#

otShortAddress otLinkGetShortAddress (otInstance * aInstance)

Get the IEEE 802.15.4 Short Address.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • A pointer to the IEEE 802.15.4 Short Address.


otLinkGetMaxFrameRetriesDirect#

uint8_t otLinkGetMaxFrameRetriesDirect (otInstance * aInstance)

This method returns the maximum number of frame retries during direct transmission.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The maximum number of retries during direct transmission.


otLinkSetMaxFrameRetriesDirect#

void otLinkSetMaxFrameRetriesDirect (otInstance * aInstance, uint8_t aMaxFrameRetriesDirect)

This method sets the maximum number of frame retries during direct transmission.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aMaxFrameRetriesDirect

The maximum number of retries during direct transmission.


otLinkGetMaxFrameRetriesIndirect#

uint8_t otLinkGetMaxFrameRetriesIndirect (otInstance * aInstance)

This method returns the maximum number of frame retries during indirect transmission.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The maximum number of retries during indirect transmission.


otLinkSetMaxFrameRetriesIndirect#

void otLinkSetMaxFrameRetriesIndirect (otInstance * aInstance, uint8_t aMaxFrameRetriesIndirect)

This method sets the maximum number of frame retries during indirect transmission.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aMaxFrameRetriesIndirect

The maximum number of retries during indirect transmission.


otLinkFilterGetAddressMode#

otMacFilterAddressMode otLinkFilterGetAddressMode (otInstance * aInstance)

This function gets the address mode of MAC filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Returns

  • the address mode.


otLinkFilterSetAddressMode#

void otLinkFilterSetAddressMode (otInstance * aInstance, otMacFilterAddressMode aMode)

This function sets the address mode of MAC filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMacFilterAddressMode[in]aMode

The address mode to set.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkFilterAddAddress#

otError otLinkFilterAddAddress (otInstance * aInstance, const otExtAddress * aExtAddress)

This method adds an Extended Address to MAC filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otExtAddress *[in]aExtAddress

A pointer to the Extended Address (MUST NOT be NULL).

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkFilterRemoveAddress#

void otLinkFilterRemoveAddress (otInstance * aInstance, const otExtAddress * aExtAddress)

This method removes an Extended Address from MAC filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otExtAddress *[in]aExtAddress

A pointer to the Extended Address (MUST NOT be NULL).

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

No action is performed if there is no existing entry in Filter matching the given Extended Address.


otLinkFilterClearAddresses#

void otLinkFilterClearAddresses (otInstance * aInstance)

This method clears all the Extended Addresses from MAC filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkFilterGetNextAddress#

otError otLinkFilterGetNextAddress (otInstance * aInstance, otMacFilterIterator * aIterator, otMacFilterEntry * aEntry)

This method gets an in-use address filter entry.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMacFilterIterator *[inout]aIterator

A pointer to the MAC filter iterator context. To get the first in-use address filter entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT. MUST NOT be NULL.

otMacFilterEntry *[out]aEntry

A pointer to where the information is placed. MUST NOT be NULL.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkFilterAddRssIn#

otError otLinkFilterAddRssIn (otInstance * aInstance, const otExtAddress * aExtAddress, int8_t aRss)

This method adds a fixed received signal strength (in dBm) entry for the messages from a given Extended Address in MAC Filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otExtAddress *[in]aExtAddress

A pointer to the IEEE 802.15.4 Extended Address. MUST NOT be NULL.

int8_t[in]aRss

A received signal strength (in dBm).

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkFilterRemoveRssIn#

void otLinkFilterRemoveRssIn (otInstance * aInstance, const otExtAddress * aExtAddress)

This method removes a MAC Filter entry for fixed received signal strength setting for a given Extended Address.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otExtAddress *[in]aExtAddress

A pointer to the IEEE 802.15.4 Extended Address. MUST NOT be NULL.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

No action is performed if there is no existing entry in Filter matching the given Extended Address.


otLinkFilterSetDefaultRssIn#

void otLinkFilterSetDefaultRssIn (otInstance * aInstance, int8_t aRss)

This method sets the default received signal strength (in dBm) on MAC Filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

int8_t[in]aRss

The default received signal strength (in dBm) to set.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

The default RSS value is used for all received frames from addresses for which there is no explicit RSS-IN entry in the Filter list (added using otLinkFilterAddRssIn()).


otLinkFilterClearDefaultRssIn#

void otLinkFilterClearDefaultRssIn (otInstance * aInstance)

This method clears any previously set default received signal strength (in dBm) on MAC Filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkFilterClearAllRssIn#

void otLinkFilterClearAllRssIn (otInstance * aInstance)

This method clears all the received signal strength entries (including default RSS-in) on MAC Filter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkFilterGetNextRssIn#

otError otLinkFilterGetNextRssIn (otInstance * aInstance, otMacFilterIterator * aIterator, otMacFilterEntry * aEntry)

This method gets an in-use RssIn filter entry.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMacFilterIterator *[inout]aIterator

A pointer to the MAC filter iterator context. MUST NOT be NULL. To get the first entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT.

otMacFilterEntry *[out]aEntry

A pointer to where the information is placed. The last entry would have the extended address as all 0xff to indicate the default received signal strength if it was set. aEntry MUST NOT be NULL.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkSetRadioFilterEnabled#

void otLinkSetRadioFilterEnabled (otInstance * aInstance, bool aFilterEnabled)

This function enables/disables IEEE 802.15.4 radio filter mode.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aFilterEnabled

TRUE to enable radio filter, FALSE to disable

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

The radio filter is mainly intended for testing. It can be used to temporarily block all tx/rx on the 802.15.4 radio. When radio filter is enabled, radio is put to sleep instead of receive (to ensure device does not receive any frame and/or potentially send ack). Also the frame transmission requests return immediately without sending the frame over the air (return "no ack" error if ack is requested, otherwise return success).


otLinkIsRadioFilterEnabled#

bool otLinkIsRadioFilterEnabled (otInstance * aInstance)

This function indicates whether the IEEE 802.15.4 radio filter is enabled or not.

Parameters
TypeDirectionArgument NameDescription
otInstance *N/AaInstance

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.


otLinkConvertRssToLinkQuality#

uint8_t otLinkConvertRssToLinkQuality (otInstance * aInstance, int8_t aRss)

This method converts received signal strength to link quality.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

int8_t[in]aRss

The received signal strength value to be converted.

Returns

  • Link quality value mapping to aRss.


otLinkConvertLinkQualityToRss#

int8_t otLinkConvertLinkQualityToRss (otInstance * aInstance, uint8_t aLinkQuality)

This method converts link quality to typical received signal strength.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aLinkQuality

LinkQuality value, should be in range [0,3].

Returns

  • Typical platform received signal strength mapping to aLinkQuality.


otLinkGetTxDirectRetrySuccessHistogram#

const uint32_t * otLinkGetTxDirectRetrySuccessHistogram (otInstance * aInstance, uint8_t * aNumberOfEntries)

This method gets histogram of retries for a single direct packet until success.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t *[out]aNumberOfEntries

A pointer to where the size of returned histogram array is placed.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.

Returns

  • A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.


otLinkGetTxIndirectRetrySuccessHistogram#

const uint32_t * otLinkGetTxIndirectRetrySuccessHistogram (otInstance * aInstance, uint8_t * aNumberOfEntries)

This method gets histogram of retries for a single indirect packet until success.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t *[out]aNumberOfEntries

A pointer to where the size of returned histogram array is placed.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.

Returns

  • A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.


otLinkResetTxRetrySuccessHistogram#

void otLinkResetTxRetrySuccessHistogram (otInstance * aInstance)

This method clears histogram statistics for direct and indirect transmissions.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.


otLinkGetCounters#

const otMacCounters * otLinkGetCounters (otInstance * aInstance)

Get the MAC layer counters.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • A pointer to the MAC layer counters.


otLinkResetCounters#

void otLinkResetCounters (otInstance * aInstance)

Resets the MAC layer counters.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otLinkSetPcapCallback#

void otLinkSetPcapCallback (otInstance * aInstance, otLinkPcapCallback aPcapCallback, void * aCallbackContext)

This function registers a callback to provide received raw IEEE 802.15.4 frames.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otLinkPcapCallback[in]aPcapCallback

A pointer to a function that is called when receiving an IEEE 802.15.4 link frame or NULL to disable the callback.

void *[in]aCallbackContext

A pointer to application-specific context.


otLinkIsPromiscuous#

bool otLinkIsPromiscuous (otInstance * aInstance)

This function indicates whether or not promiscuous mode is enabled at the link layer.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otLinkSetPromiscuous#

otError otLinkSetPromiscuous (otInstance * aInstance, bool aPromiscuous)

This function enables or disables the link layer promiscuous mode.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aPromiscuous

true to enable promiscuous mode, or false otherwise.

Note

  • Promiscuous mode may only be enabled when the Thread interface is disabled.


otLinkCslGetChannel#

uint8_t otLinkCslGetChannel (otInstance * aInstance)

This function gets the CSL channel.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The CSL channel.


otLinkCslSetChannel#

otError otLinkCslSetChannel (otInstance * aInstance, uint8_t aChannel)

Sets the CSL channel.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aChannel

The CSL sample channel. Channel value should be 0 (Set CSL Channel unspecified) or within the range [1, 10] (if 915-MHz supported) and [11, 26] (if 2.4 GHz supported).


otLinkCslGetPeriod#

uint16_t otLinkCslGetPeriod (otInstance * aInstance)

This function gets the CSL period.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The CSL period in units of 10 symbols.


otLinkCslSetPeriod#

otError otLinkCslSetPeriod (otInstance * aInstance, uint16_t aPeriod)

Sets the CSL period in units of 10 symbols.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aPeriod

The CSL period in units of 10 symbols.

Disable CSL by setting this parameter to 0.


otLinkCslGetTimeout#

uint32_t otLinkCslGetTimeout (otInstance * aInstance)

This function gets the CSL timeout.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The CSL timeout in seconds.


otLinkCslSetTimeout#

otError otLinkCslSetTimeout (otInstance * aInstance, uint32_t aTimeout)

Sets the CSL timeout in seconds.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aTimeout

The CSL timeout in seconds.


otLinkGetCcaFailureRate#

uint16_t otLinkGetCcaFailureRate (otInstance * aInstance)

This function returns the current CCA (Clear Channel Assessment) failure rate.

Parameters
TypeDirectionArgument NameDescription
otInstance *N/AaInstance

The rate is maintained over a window of (roughly) last OPENTHREAD_CONFIG_CCA_FAILURE_RATE_AVERAGING_WINDOW frame transmissions.

Returns

  • The CCA failure rate with maximum value 0xffff corresponding to 100% failure rate.


otLinkSetEnabled#

otError otLinkSetEnabled (otInstance * aInstance, bool aEnable)

This function enables or disables the link layer.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aEnable

true to enable the link layer, or false otherwise.

Note

  • The link layer may only be enabled / disabled when the Thread Interface is disabled.


otLinkIsEnabled#

bool otLinkIsEnabled (otInstance * aInstance)

This function indicates whether or not the link layer is enabled.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otLinkSendEmptyData#

otError otLinkSendEmptyData (otInstance * aInstance)

This function instructs the device to send an empty IEEE 802.15.4 data frame.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

This function is only supported on an Rx-Off-When-Idle device to send an empty data frame to its parent. Note: available only when OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE is enabled.


Macro Definition Documentation#

OT_US_PER_TEN_SYMBOLS#

#define OT_US_PER_TEN_SYMBOLS
Value:
OT_RADIO_TEN_SYMBOLS_TIME

Time for 10 symbols in units of microseconds.


OT_MAC_FILTER_FIXED_RSS_DISABLED#

#define OT_MAC_FILTER_FIXED_RSS_DISABLED
Value:
127

Used to indicate no fixed received signal strength was set.


OT_MAC_FILTER_ITERATOR_INIT#

#define OT_MAC_FILTER_ITERATOR_INIT
Value:
0

Initializer for otMacFilterIterator.