This structure represents link-specific information for messages received from the Thread radio.

Public Attributes#

uint16_t

Source PAN ID.

uint8_t

802.15.4 Channel

int8_t

Received Signal Strength in dBm.

uint8_t

Link Quality Indicator for a received message.

bool

Indicates whether or not link security is enabled.

bool

Indicates whether or not destination PAN ID is broadcast.

uint8_t

The time sync sequence.

int64_t

The time offset to the Thread network time, in microseconds.

uint8_t

Radio link type.

Public Attribute Documentation#

mPanId#

uint16_t otThreadLinkInfo::mPanId

Source PAN ID.


mChannel#

uint8_t otThreadLinkInfo::mChannel

802.15.4 Channel


mRss#

int8_t otThreadLinkInfo::mRss

Received Signal Strength in dBm.


mLqi#

uint8_t otThreadLinkInfo::mLqi

Link Quality Indicator for a received message.


mLinkSecurity#

bool otThreadLinkInfo::mLinkSecurity

Indicates whether or not link security is enabled.


mIsDstPanIdBroadcast#

bool otThreadLinkInfo::mIsDstPanIdBroadcast

Indicates whether or not destination PAN ID is broadcast.


mTimeSyncSeq#

uint8_t otThreadLinkInfo::mTimeSyncSeq

The time sync sequence.


mNetworkTimeOffset#

int64_t otThreadLinkInfo::mNetworkTimeOffset

The time offset to the Thread network time, in microseconds.


mRadioType#

uint8_t otThreadLinkInfo::mRadioType

Radio link type.