This structure contains the counters of DNS-SD server.

Public Attributes#

uint32_t

The number of successful responses.

uint32_t

The number of server failure responses.

uint32_t

The number of format error responses.

uint32_t

The number of name error responses.

uint32_t

The number of 'not implemented' responses.

uint32_t

The number of other responses.

uint32_t

The number of queries completely resolved by the local SRP server.

Public Attribute Documentation#

mSuccessResponse#

uint32_t otDnssdCounters::mSuccessResponse

The number of successful responses.


mServerFailureResponse#

uint32_t otDnssdCounters::mServerFailureResponse

The number of server failure responses.


mFormatErrorResponse#

uint32_t otDnssdCounters::mFormatErrorResponse

The number of format error responses.


mNameErrorResponse#

uint32_t otDnssdCounters::mNameErrorResponse

The number of name error responses.


mNotImplementedResponse#

uint32_t otDnssdCounters::mNotImplementedResponse

The number of 'not implemented' responses.


mOtherResponse#

uint32_t otDnssdCounters::mOtherResponse

The number of other responses.


mResolvedBySrp#

uint32_t otDnssdCounters::mResolvedBySrp

The number of queries completely resolved by the local SRP server.