This structure represents a neighbor info.
Public Attributes#
Neighbor's Extended Address.
uint16_t
Neighbor's RLOC16.
int8_t
Average RSSI of rx frames from neighbor at the time of recording entry.
uint8_t
Indicates the event (OT_HISTORY_TRACKER_NEIGHBOR_EVENT_* enumeration).
bool
Rx-on-when-idle.
bool
Full Thread Device.
bool
Full Network Data.
bool
Indicates whether or not the neighbor is a child.
Public Attribute Documentation#
mAverageRssi#
int8_t otHistoryTrackerNeighborInfo::mAverageRssi
Average RSSI of rx frames from neighbor at the time of recording entry.
mEvent#
uint8_t otHistoryTrackerNeighborInfo::mEvent
Indicates the event (OT_HISTORY_TRACKER_NEIGHBOR_EVENT_* enumeration).
mIsChild#
bool otHistoryTrackerNeighborInfo::mIsChild
Indicates whether or not the neighbor is a child.