The following are valid radio state transitions:

                               (Radio ON)

+-------—+ Enable() +----—+ Receive() +------—+ Transmit() +-------—+ | |--------—>| |--------—>| |-----------—>| | | Disabled | | Sleep | | Receive | | Transmit | | |<--------—| |<--------—| |<-----------—| | +-------—+ Disable() +----—+ Sleep() +------—+ Receive() +-------—+ (Radio OFF) or signal TransmitDone

During the IEEE 802.15.4 data request command the transition Sleep->Receive->Transmit can be shortened to direct transition from Sleep to Transmit if the platform supports the OT_RADIO_CAPS_SLEEP_TO_TX capability. This structure represents radio coexistence metrics.

Public Attributes#

uint32_t

Number of grant glitches.

uint32_t

Number of tx requests.

uint32_t

Number of tx requests while grant was active.

uint32_t

Number of tx requests while grant was inactive.

uint32_t

Number of tx requests while grant was inactive that were ultimately granted.

uint32_t

Number of tx requests while grant was inactive that timed out.

uint32_t

Number of tx that were in progress when grant was deactivated.

uint32_t

Number of tx requests that were not granted within 50us.

uint32_t

Average time in usec from tx request to grant.

uint32_t

Number of rx requests.

uint32_t

Number of rx requests while grant was active.

uint32_t

Number of rx requests while grant was inactive.

uint32_t

Number of rx requests while grant was inactive that were ultimately granted.

uint32_t

Number of rx requests while grant was inactive that timed out.

uint32_t

Number of rx that were in progress when grant was deactivated.

uint32_t

Number of rx requests that were not granted within 50us.

uint32_t

Average time in usec from rx request to grant.

uint32_t

Number of rx requests that completed without receiving grant.

bool

Stats collection stopped due to saturation.

Public Attribute Documentation#

mNumGrantGlitch#

uint32_t otRadioCoexMetrics::mNumGrantGlitch

Number of grant glitches.


mNumTxRequest#

uint32_t otRadioCoexMetrics::mNumTxRequest

Number of tx requests.


mNumTxGrantImmediate#

uint32_t otRadioCoexMetrics::mNumTxGrantImmediate

Number of tx requests while grant was active.


mNumTxGrantWait#

uint32_t otRadioCoexMetrics::mNumTxGrantWait

Number of tx requests while grant was inactive.


mNumTxGrantWaitActivated#

uint32_t otRadioCoexMetrics::mNumTxGrantWaitActivated

Number of tx requests while grant was inactive that were ultimately granted.


mNumTxGrantWaitTimeout#

uint32_t otRadioCoexMetrics::mNumTxGrantWaitTimeout

Number of tx requests while grant was inactive that timed out.


mNumTxGrantDeactivatedDuringRequest#

uint32_t otRadioCoexMetrics::mNumTxGrantDeactivatedDuringRequest

Number of tx that were in progress when grant was deactivated.


mNumTxDelayedGrant#

uint32_t otRadioCoexMetrics::mNumTxDelayedGrant

Number of tx requests that were not granted within 50us.


mAvgTxRequestToGrantTime#

uint32_t otRadioCoexMetrics::mAvgTxRequestToGrantTime

Average time in usec from tx request to grant.


mNumRxRequest#

uint32_t otRadioCoexMetrics::mNumRxRequest

Number of rx requests.


mNumRxGrantImmediate#

uint32_t otRadioCoexMetrics::mNumRxGrantImmediate

Number of rx requests while grant was active.


mNumRxGrantWait#

uint32_t otRadioCoexMetrics::mNumRxGrantWait

Number of rx requests while grant was inactive.


mNumRxGrantWaitActivated#

uint32_t otRadioCoexMetrics::mNumRxGrantWaitActivated

Number of rx requests while grant was inactive that were ultimately granted.


mNumRxGrantWaitTimeout#

uint32_t otRadioCoexMetrics::mNumRxGrantWaitTimeout

Number of rx requests while grant was inactive that timed out.


mNumRxGrantDeactivatedDuringRequest#

uint32_t otRadioCoexMetrics::mNumRxGrantDeactivatedDuringRequest

Number of rx that were in progress when grant was deactivated.


mNumRxDelayedGrant#

uint32_t otRadioCoexMetrics::mNumRxDelayedGrant

Number of rx requests that were not granted within 50us.


mAvgRxRequestToGrantTime#

uint32_t otRadioCoexMetrics::mAvgRxRequestToGrantTime

Average time in usec from rx request to grant.


mNumRxGrantNone#

uint32_t otRadioCoexMetrics::mNumRxGrantNone

Number of rx requests that completed without receiving grant.


mStopped#

bool otRadioCoexMetrics::mStopped

Stats collection stopped due to saturation.