This structure represents an IEEE 802.15.4 radio frame.
Public Attributes#
The PSDU.
Length of the PSDU.
Channel used to transmit/receive the frame.
Radio link type - should be ignored by radio driver.
Interface Id for the incoming/outgoing radio packet.
The key material used for AES-CCM frame security.
The pointer to the Header IE(s) related information.
The delay time for this transmission (based on mTxDelayBaseTime).
The base time for the transmission delay.
Maximum number of backoffs attempts before declaring CCA failure.
Maximum number of retries allowed after a transmission failure.
The RX channel after frame TX is done (after all frame retries - ack received, or timeout, or abort).
Indicates whether frame counter and CSL IEs are properly updated in the header.
Indicates whether the frame is a retransmission or not.
Set to true to enable CSMA-CA for this packet, false otherwise.
Set to true if CSL header IE is present.
True if SubMac should skip the AES processing of this frame.
Structure representing radio frame transmit information.
The timestamp when the frame was received in microseconds.
ACK security frame counter (applicable when mAckedWithSecEnhAck is set).
ACK security key index (applicable when mAckedWithSecEnhAck is set).
Received signal strength indicator in dBm for received frames.
Link Quality Indicator for received frames.
This indicates if this frame was acknowledged with frame pending set.
This indicates if this frame was acknowledged with secured enhance ACK.
Structure representing radio frame receive information.
The union of transmit and receive information for a radio frame.
Public Attribute Documentation#
mIid#
uint8_t otRadioFrame::mIid
Interface Id for the incoming/outgoing radio packet.
This field is used by RCP when OPENTHREAD_CONFIG_MULTIPAN_RCP_ENABLE is enabled. If not enabled, this field defaults to zero.
Incoming packets are marked with the correct IID to deliver to the appropriate host. RCP determines the IID value based on the destination PAN ID of the received packet. The IID value of zero indicates the broadcast packet, which will send it to all the hosts.
For outgoing packets, IID is used to format the transmit done callback for the appropriate host. RCP extracts the IID value while processing the received spinel frame from the spinel header.
mAesKey#
const otMacKeyMaterial* otRadioFrame::mAesKey
The key material used for AES-CCM frame security.
mTxDelay#
uint32_t otRadioFrame::mTxDelay
The delay time for this transmission (based on mTxDelayBaseTime).
mMaxCsmaBackoffs#
uint8_t otRadioFrame::mMaxCsmaBackoffs
Maximum number of backoffs attempts before declaring CCA failure.
mMaxFrameRetries#
uint8_t otRadioFrame::mMaxFrameRetries
Maximum number of retries allowed after a transmission failure.
mRxChannelAfterTxDone#
uint8_t otRadioFrame::mRxChannelAfterTxDone
The RX channel after frame TX is done (after all frame retries - ack received, or timeout, or abort).
Radio platforms can choose to fully ignore this. OT stack will make sure to call otPlatRadioReceive() with the desired RX channel after a frame TX is done and signaled in otPlatRadioTxDone() callback. Radio platforms that don't provide OT_RADIO_CAPS_TRANSMIT_RETRIES must always ignore this.
This is intended for situations where there may be delay in interactions between OT stack and radio, as an example this is used in RCP/host architecture to make sure RCP switches to PAN channel more quickly. In particular, this can help with CSL tx to a sleepy child, where the child may use a different channel for CSL than the PAN channel. After frame tx, we want the radio/RCP to go back to the PAN channel quickly to ensure that parent does not miss tx from child afterwards, e.g., child responding to the earlier CSL transmitted frame from parent using PAN channel while radio still staying on CSL channel.
The switch to the RX channel MUST happen after the frame TX is fully done, i.e., after all retries and when ack is received (when "Ack Request" flag is set on the TX frame) or ack timeout. Note that ack is expected on the same channel that frame is sent on.
mIsHeaderUpdated#
bool otRadioFrame::mIsHeaderUpdated
Indicates whether frame counter and CSL IEs are properly updated in the header.
If the platform layer does not provide OT_RADIO_CAPS_TRANSMIT_SEC capability, it can ignore this flag.
If the platform provides OT_RADIO_CAPS_TRANSMIT_SEC capability, then platform is expected to handle tx security processing and assignment of frame counter. In this case the following behavior is expected:
When mIsHeaderUpdated is set, it indicates that OpenThread core has already set the frame counter and CSL IEs (if security is enabled) in the prepared frame. The counter is ensured to match the counter value from the previous attempts of the same frame. The platform should not assign or change the frame counter (but may still need to perform security processing depending on mIsSecurityProcessed flag).
If mIsHeaderUpdated is not set, then the frame counter and key CSL IE not set in the frame by OpenThread core and it is the responsibility of the radio platform to assign them. The platform must update the frame header (assign counter and CSL IE values) before sending the frame over the air, however if the the transmission gets aborted and the frame is never sent over the air (e.g., channel access error) the platform may choose to not update the header. If the platform updates the header, it must also set this flag before passing the frame back from the otPlatRadioTxDone() callback.
mCsmaCaEnabled#
bool otRadioFrame::mCsmaCaEnabled
Set to true to enable CSMA-CA for this packet, false otherwise.
mIsSecurityProcessed#
bool otRadioFrame::mIsSecurityProcessed
True if SubMac should skip the AES processing of this frame.
mTxInfo#
struct otRadioFrame::@19::@20 otRadioFrame::mTxInfo
Structure representing radio frame transmit information.
mTimestamp#
uint64_t otRadioFrame::mTimestamp
The timestamp when the frame was received in microseconds.
The value SHALL be the time when the SFD was received.
mAckFrameCounter#
uint32_t otRadioFrame::mAckFrameCounter
ACK security frame counter (applicable when mAckedWithSecEnhAck is set).
mAckKeyId#
uint8_t otRadioFrame::mAckKeyId
ACK security key index (applicable when mAckedWithSecEnhAck is set).
mAckedWithFramePending#
bool otRadioFrame::mAckedWithFramePending
This indicates if this frame was acknowledged with frame pending set.
mAckedWithSecEnhAck#
bool otRadioFrame::mAckedWithSecEnhAck
This indicates if this frame was acknowledged with secured enhance ACK.
mRxInfo#
struct otRadioFrame::@19::@21 otRadioFrame::mRxInfo
Structure representing radio frame receive information.
mInfo#
union otRadioFrame::@19 otRadioFrame::mInfo
The union of transmit and receive information for a radio frame.