This structure includes SRP server LEASE and KEY-LEASE configurations.

Public Attributes#

uint32_t

The minimum LEASE interval in seconds.

uint32_t

The maximum LEASE interval in seconds.

uint32_t

The minimum KEY-LEASE interval in seconds.

uint32_t

The maximum KEY-LEASE interval in seconds.

Public Attribute Documentation#

mMinLease#

uint32_t otSrpServerLeaseConfig::mMinLease

The minimum LEASE interval in seconds.


mMaxLease#

uint32_t otSrpServerLeaseConfig::mMaxLease

The maximum LEASE interval in seconds.


mMinKeyLease#

uint32_t otSrpServerLeaseConfig::mMinKeyLease

The minimum KEY-LEASE interval in seconds.


mMaxKeyLease#

uint32_t otSrpServerLeaseConfig::mMaxKeyLease

The maximum KEY-LEASE interval in seconds.