This structure includes the statistics of SRP server responses.

Public Attributes#

uint32_t

The number of successful responses.

uint32_t

The number of server failure responses.

uint32_t

The number of format error responses.

uint32_t

The number of 'name exists' responses.

uint32_t

The number of refused responses.

uint32_t

The number of other responses.

Public Attribute Documentation#

mSuccess#

uint32_t otSrpServerResponseCounters::mSuccess

The number of successful responses.


mServerFailure#

uint32_t otSrpServerResponseCounters::mServerFailure

The number of server failure responses.


mFormatError#

uint32_t otSrpServerResponseCounters::mFormatError

The number of format error responses.


mNameExists#

uint32_t otSrpServerResponseCounters::mNameExists

The number of 'name exists' responses.


mRefused#

uint32_t otSrpServerResponseCounters::mRefused

The number of refused responses.


mOther#

uint32_t otSrpServerResponseCounters::mOther

The number of other responses.