This structure represents a TCP listener.
A TCP listener is used to listen for and accept incoming TCP connections.
The application should not inspect the fields of this structure directly; it should only interact with it via the TCP API functions whose signatures are provided in this file.
Public Attributes#
uint8_t
void *
union otTcpListener::@28
struct otTcpListener *
A pointer to the next TCP listener (internal use only)
void *
A pointer to application-specific context.
"Accept ready" callback function
"Accept done" callback function
Public Attribute Documentation#
mSize#
uint8_t otTcpListener::mSize[OT_TCP_LISTENER_TCB_SIZE_BASE+OT_TCP_LISTENER_TCB_NUM_PTR *sizeof(void *)]
mNext#
struct otTcpListener* otTcpListener::mNext
A pointer to the next TCP listener (internal use only)
mAcceptReadyCallback#
otTcpAcceptReady otTcpListener::mAcceptReadyCallback
"Accept ready" callback function
mAcceptDoneCallback#
otTcpAcceptDone otTcpListener::mAcceptDoneCallback
"Accept done" callback function