You are viewing documentation for version:
Represents the Key Material required for Crypto operations.
Public Attributes#
const uint8_t *
Pointer to the buffer containing key. NULL indicates to use mKeyRef.
uint16_t
The key length in bytes (applicable when mKey is not NULL).
uint32_t
The PSA key ref (requires mKey to be NULL).
Public Attribute Documentation#
mKey#
const uint8_t* otCryptoKey::mKey
Pointer to the buffer containing key. NULL indicates to use mKeyRef.
mKeyLength#
uint16_t otCryptoKey::mKeyLength
The key length in bytes (applicable when mKey is not NULL).
mKeyRef#
uint32_t otCryptoKey::mKeyRef
The PSA key ref (requires mKey to be NULL).