Factory Diagnostics - Platform#
This module includes the platform abstraction for diagnostics features.
Enumerations#
Functions#
Processes a factory diagnostics command line.
Enables/disables the factory diagnostics mode.
Indicates whether or not factory diagnostics mode is enabled.
Sets the channel to use for factory diagnostics.
Sets the transmit power to use for factory diagnostics.
Processes the received radio frame.
Processes the alarm event.
Sets the gpio value.
Gets the gpio value.
Sets the gpio mode.
Gets the gpio mode.
Set the radio raw power setting for diagnostics module.
Get the radio raw power setting for diagnostics module.
Enable/disable the platform layer to use the raw power setting set by otPlatDiagRadioSetRawPowerSetting().
Start/stop the platform layer to transmit continuous carrier wave.
Start/stop the platform layer to transmit stream of characters.
Get the power settings for the given channel.
Enumeration Documentation#
otGpioMode#
otGpioMode
Defines the gpio modes.
| Enumerator | |
|---|---|
| OT_GPIO_MODE_INPUT | Input mode without pull resistor. |
| OT_GPIO_MODE_OUTPUT | Output mode. |
Function Documentation#
otPlatDiagProcess#
otError otPlatDiagProcess (otInstance * aInstance, uint8_t aArgsLength, char * aArgs, char * aOutput, size_t aOutputMaxLen)
Processes a factory diagnostics command line.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance for current request. |
| uint8_t | [in] | aArgsLength | The number of arguments in |
| char * | [in] | aArgs | The arguments of diagnostics command line. |
| char * | [out] | aOutput | The diagnostics execution result. |
| size_t | [in] | aOutputMaxLen | The output buffer size. |
The output of this function (the content written to aOutput) MUST terminate with \0 and the \0 is within the output buffer.
otPlatDiagModeSet#
void otPlatDiagModeSet (bool aMode)
Enables/disables the factory diagnostics mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | aMode | TRUE to enable diagnostics mode, FALSE otherwise. |
otPlatDiagModeGet#
bool otPlatDiagModeGet (void )
Indicates whether or not factory diagnostics mode is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
TRUE if factory diagnostics mode is enabled, FALSE otherwise.
otPlatDiagChannelSet#
void otPlatDiagChannelSet (uint8_t aChannel)
Sets the channel to use for factory diagnostics.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | aChannel | The channel value. |
otPlatDiagTxPowerSet#
void otPlatDiagTxPowerSet (int8_t aTxPower)
Sets the transmit power to use for factory diagnostics.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int8_t | [in] | aTxPower | The transmit power value. |
otPlatDiagRadioReceived#
void otPlatDiagRadioReceived (otInstance * aInstance, otRadioFrame * aFrame, otError aError)
Processes the received radio frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance for current request. |
| otRadioFrame * | [in] | aFrame | The received radio frame. |
| otError | [in] | aError | The received radio frame status. |
otPlatDiagAlarmCallback#
void otPlatDiagAlarmCallback (otInstance * aInstance)
Processes the alarm event.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance for current request. |
otPlatDiagGpioSet#
otError otPlatDiagGpioSet (uint32_t aGpio, bool aValue)
Sets the gpio value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | aGpio | The gpio number. |
| bool | [in] | aValue | true to set the gpio to high level, or false otherwise. |
otPlatDiagGpioGet#
otError otPlatDiagGpioGet (uint32_t aGpio, bool * aValue)
Gets the gpio value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | aGpio | The gpio number. |
| bool * | [out] | aValue | A pointer where to put gpio value. |
otPlatDiagGpioSetMode#
otError otPlatDiagGpioSetMode (uint32_t aGpio, otGpioMode aMode)
Sets the gpio mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | aGpio | The gpio number. |
| otGpioMode | [out] | aMode | The gpio mode. |
otPlatDiagGpioGetMode#
otError otPlatDiagGpioGetMode (uint32_t aGpio, otGpioMode * aMode)
Gets the gpio mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | aGpio | The gpio number. |
| otGpioMode * | [out] | aMode | A pointer where to put gpio mode. |
otPlatDiagRadioSetRawPowerSetting#
otError otPlatDiagRadioSetRawPowerSetting (otInstance * aInstance, const uint8_t * aRawPowerSetting, uint16_t aRawPowerSettingLength)
Set the radio raw power setting for diagnostics module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| const uint8_t * | [in] | aRawPowerSetting | A pointer to the raw power setting byte array. |
| uint16_t | [in] | aRawPowerSettingLength | The length of the |
otPlatDiagRadioGetRawPowerSetting#
otError otPlatDiagRadioGetRawPowerSetting (otInstance * aInstance, uint8_t * aRawPowerSetting, uint16_t * aRawPowerSettingLength)
Get the radio raw power setting for diagnostics module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint8_t * | [out] | aRawPowerSetting | A pointer to the raw power setting byte array. |
| uint16_t * | [inout] | aRawPowerSettingLength | On input, a pointer to the size of |
otPlatDiagRadioRawPowerSettingEnable#
otError otPlatDiagRadioRawPowerSettingEnable (otInstance * aInstance, bool aEnable)
Enable/disable the platform layer to use the raw power setting set by otPlatDiagRadioSetRawPowerSetting().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| bool | [in] | aEnable | TRUE to enable or FALSE to disable the raw power setting. |
otPlatDiagRadioTransmitCarrier#
otError otPlatDiagRadioTransmitCarrier (otInstance * aInstance, bool aEnable)
Start/stop the platform layer to transmit continuous carrier wave.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| bool | [in] | aEnable | TRUE to enable or FALSE to disable the platform layer to transmit continuous carrier wave. |
otPlatDiagRadioTransmitStream#
otError otPlatDiagRadioTransmitStream (otInstance * aInstance, bool aEnable)
Start/stop the platform layer to transmit stream of characters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| bool | [in] | aEnable | TRUE to enable or FALSE to disable the platform layer to transmit stream. |
otPlatDiagRadioGetPowerSettings#
otError otPlatDiagRadioGetPowerSettings (otInstance * aInstance, uint8_t aChannel, int16_t * aTargetPower, int16_t * aActualPower, uint8_t * aRawPowerSetting, uint16_t * aRawPowerSettingLength)
Get the power settings for the given channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint8_t | [in] | aChannel | The radio channel. |
| int16_t * | [out] | aTargetPower | The target power in 0.01 dBm. |
| int16_t * | [out] | aActualPower | The actual power in 0.01 dBm. |
| uint8_t * | [out] | aRawPowerSetting | A pointer to the raw power setting byte array. |
| uint16_t * | [inout] | aRawPowerSettingLength | On input, a pointer to the size of |