Represents information about a router neighbor entry from otMeshDiagQueryRouterNeighborTable().
mSupportsErrRate indicates whether or not the error tracking feature is supported and mFrameErrorRate and mMessageErrorRate values are valid. The frame error rate tracks frame tx errors (towards the child) at MAC layer, while mMessageErrorRate tracks the IPv6 message error rate (above MAC layer and after MAC retries) when an IPv6 message is dropped. For example, if the message is large and requires 6LoWPAN fragmentation, message tx is considered as failed if one of its fragment frame tx fails (for example, never acked).
Public Attributes#
mFrameErrorRate and mMessageErrorRate values are valid.
RLOC16.
Extended Address.
Version.
Seconds since link establishment.
Link Margin in dB.
Average RSSI.
RSSI of last received frame.
Frame error rate (0x0000->0%, 0xffff->100%).
(IPv6) msg error rate (0x0000->0%, 0xffff->100%).
Public Attribute Documentation#
mSupportsErrRate#
bool otMeshDiagRouterNeighborEntry::mSupportsErrRate
mFrameErrorRate and mMessageErrorRate values are valid.
mConnectionTime#
uint32_t otMeshDiagRouterNeighborEntry::mConnectionTime
Seconds since link establishment.
mFrameErrorRate#
uint16_t otMeshDiagRouterNeighborEntry::mFrameErrorRate
Frame error rate (0x0000->0%, 0xffff->100%).
mMessageErrorRate#
uint16_t otMeshDiagRouterNeighborEntry::mMessageErrorRate
(IPv6) msg error rate (0x0000->0%, 0xffff->100%).