Represents a Commissioning Dataset.
Public Attributes#
uint16_t
Border Router RLOC16.
uint16_t
Commissioner Session Id.
Steering Data.
uint16_t
Joiner UDP Port.
bool
TRUE if Border Router RLOC16 is set, FALSE otherwise.
bool
TRUE if Commissioner Session Id is set, FALSE otherwise.
bool
TRUE if Steering Data is set, FALSE otherwise.
bool
TRUE if Joiner UDP Port is set, FALSE otherwise.
Public Attribute Documentation#
mLocator#
uint16_t otCommissioningDataset::mLocator
Border Router RLOC16.
Definition at line
105
of file include/openthread/commissioner.h
mSessionId#
uint16_t otCommissioningDataset::mSessionId
Commissioner Session Id.
Definition at line
106
of file include/openthread/commissioner.h
mSteeringData#
otSteeringData otCommissioningDataset::mSteeringData
Steering Data.
Definition at line
107
of file include/openthread/commissioner.h
mJoinerUdpPort#
uint16_t otCommissioningDataset::mJoinerUdpPort
Joiner UDP Port.
Definition at line
108
of file include/openthread/commissioner.h
mIsLocatorSet#
bool otCommissioningDataset::mIsLocatorSet
TRUE if Border Router RLOC16 is set, FALSE otherwise.
Definition at line
110
of file include/openthread/commissioner.h
mIsSessionIdSet#
bool otCommissioningDataset::mIsSessionIdSet
TRUE if Commissioner Session Id is set, FALSE otherwise.
Definition at line
111
of file include/openthread/commissioner.h
mIsSteeringDataSet#
bool otCommissioningDataset::mIsSteeringDataSet
TRUE if Steering Data is set, FALSE otherwise.
Definition at line
112
of file include/openthread/commissioner.h
mIsJoinerUdpPortSet#
bool otCommissioningDataset::mIsJoinerUdpPortSet
TRUE if Joiner UDP Port is set, FALSE otherwise.
Definition at line
113
of file include/openthread/commissioner.h