History Tracker#
Records the history of different events, for example RX and TX messages or network info changes.
All tracked entries are timestamped.
The functions in this module are available when OPENTHREAD_CONFIG_HISTORY_TRACKER_ENABLE is enabled.
Modules#
otHistoryTrackerUnicastAddressInfo
otHistoryTrackerMulticastAddressInfo
otHistoryTrackerOnMeshPrefixInfo
otHistoryTrackerExternalRouteInfo
Enumerations#
Defines the events for an IPv6 (unicast or multicast) address info (i.e., whether address is added or removed).
Constants representing message priority used in otHistoryTrackerMessageInfo struct.
Defines the events in a neighbor info (i.e.
Defines the events in a router info (i.e.
Defines the events for a Network Data entry (i.e., whether an entry is added or removed).
Typedefs#
Represents an iterator to iterate through a history list.
Represents Thread network info.
Represent a unicast IPv6 address info.
Represent an IPv6 multicast address info.
Represents a RX/TX IPv6 message info.
Represents a neighbor info.
Represents a router table entry event.
Represent a Network Data on mesh prefix info.
Represent a Network Data extern route info.
Functions#
Initializes an otHistoryTrackerIterator.
Iterates over the entries in the network info history list.
Iterates over the entries in the unicast address history list.
Iterates over the entries in the multicast address history list.
Iterates over the entries in the RX message history list.
Iterates over the entries in the TX message history list.
Iterates over the entries in the neighbor history list.
Iterates over the entries in the router history list.
Iterates over the entries in the Network Data on mesh prefix entry history list.
Iterates over the entries in the Network Data external route entry history list.
Converts a given entry age to a human-readable string.
Macros#
This constant specifies the maximum age of entries which is 49 days (in msec).
Recommended size for string representation of an entry age.
No next hop - For mNextHop in otHistoryTrackerRouterInfo.
Infinite path cost - used in otHistoryTrackerRouterInfo.
Enumeration Documentation#
otHistoryTrackerAddressEvent#
otHistoryTrackerAddressEvent
Defines the events for an IPv6 (unicast or multicast) address info (i.e., whether address is added or removed).
| Enumerator | |
|---|---|
| OT_HISTORY_TRACKER_ADDRESS_EVENT_ADDED | Address is added. |
| OT_HISTORY_TRACKER_ADDRESS_EVENT_REMOVED | Address is removed. |
@1#
@1
Constants representing message priority used in otHistoryTrackerMessageInfo struct.
| Enumerator | |
|---|---|
| OT_HISTORY_TRACKER_MSG_PRIORITY_LOW | Low priority level. |
| OT_HISTORY_TRACKER_MSG_PRIORITY_NORMAL | Normal priority level. |
| OT_HISTORY_TRACKER_MSG_PRIORITY_HIGH | High priority level. |
| OT_HISTORY_TRACKER_MSG_PRIORITY_NET | Network Control priority level. |
otHistoryTrackerNeighborEvent#
otHistoryTrackerNeighborEvent
Defines the events in a neighbor info (i.e.
whether neighbor is added, removed, or changed).
Event OT_HISTORY_TRACKER_NEIGHBOR_EVENT_RESTORING is applicable to child neighbors only. It is triggered after the device (re)starts and when the previous children list is retrieved from non-volatile settings and the device tries to restore connection to them.
| Enumerator | |
|---|---|
| OT_HISTORY_TRACKER_NEIGHBOR_EVENT_ADDED | Neighbor is added. |
| OT_HISTORY_TRACKER_NEIGHBOR_EVENT_REMOVED | Neighbor is removed. |
| OT_HISTORY_TRACKER_NEIGHBOR_EVENT_CHANGED | Neighbor changed (e.g., device mode flags changed). |
| OT_HISTORY_TRACKER_NEIGHBOR_EVENT_RESTORING | Neighbor is being restored (applicable to child only). |
otHistoryTrackerRouterEvent#
otHistoryTrackerRouterEvent
Defines the events in a router info (i.e.
whether router is added, removed, or changed).
| Enumerator | |
|---|---|
| OT_HISTORY_TRACKER_ROUTER_EVENT_ADDED | Router is added (router ID allocated). |
| OT_HISTORY_TRACKER_ROUTER_EVENT_REMOVED | Router entry is removed (router ID released). |
| OT_HISTORY_TRACKER_ROUTER_EVENT_NEXT_HOP_CHANGED | Router entry next hop and cost changed. |
| OT_HISTORY_TRACKER_ROUTER_EVENT_COST_CHANGED | Router entry path cost changed (next hop as before). |
otHistoryTrackerNetDataEvent#
otHistoryTrackerNetDataEvent
Defines the events for a Network Data entry (i.e., whether an entry is added or removed).
| Enumerator | |
|---|---|
| OT_HISTORY_TRACKER_NET_DATA_ENTRY_ADDED | Network data entry is added. |
| OT_HISTORY_TRACKER_NET_DATA_ENTRY_REMOVED | Network data entry is removed. |
Typedef Documentation#
otHistoryTrackerIterator#
typedef struct otHistoryTrackerIterator otHistoryTrackerIterator
Represents an iterator to iterate through a history list.
The fields in this type are opaque (intended for use by OpenThread core) and therefore should not be accessed/used by caller.
Before using an iterator, it MUST be initialized using otHistoryTrackerInitIterator(),
otHistoryTrackerNetworkInfo#
typedef struct otHistoryTrackerNetworkInfo otHistoryTrackerNetworkInfo
Represents Thread network info.
otHistoryTrackerUnicastAddressInfo#
typedef struct otHistoryTrackerUnicastAddressInfo otHistoryTrackerUnicastAddressInfo
Represent a unicast IPv6 address info.
otHistoryTrackerMulticastAddressInfo#
typedef struct otHistoryTrackerMulticastAddressInfo otHistoryTrackerMulticastAddressInfo
Represent an IPv6 multicast address info.
otHistoryTrackerMessageInfo#
typedef struct otHistoryTrackerMessageInfo otHistoryTrackerMessageInfo
Represents a RX/TX IPv6 message info.
Some of the fields in this struct are applicable to a RX message or a TX message only, e.g., mAveRxRss is the average RSS of all fragment frames that form a received message and is only applicable for a RX message.
otHistoryTrackerNeighborInfo#
typedef struct otHistoryTrackerNeighborInfo otHistoryTrackerNeighborInfo
Represents a neighbor info.
otHistoryTrackerRouterInfo#
typedef struct otHistoryTrackerRouterInfo otHistoryTrackerRouterInfo
Represents a router table entry event.
otHistoryTrackerOnMeshPrefixInfo#
typedef struct otHistoryTrackerOnMeshPrefixInfo otHistoryTrackerOnMeshPrefixInfo
Represent a Network Data on mesh prefix info.
otHistoryTrackerExternalRouteInfo#
typedef struct otHistoryTrackerExternalRouteInfo otHistoryTrackerExternalRouteInfo
Represent a Network Data extern route info.
Function Documentation#
otHistoryTrackerInitIterator#
void otHistoryTrackerInitIterator (otHistoryTrackerIterator * aIterator)
Initializes an otHistoryTrackerIterator.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otHistoryTrackerIterator * | [in] | aIterator | A pointer to the iterator to initialize (MUST NOT be NULL). |
An iterator MUST be initialized before it is used.
An iterator can be initialized again to start from the beginning of the list.
When iterating over entries in a list, to ensure the entry ages are consistent, the age is given relative to the time the iterator was initialized, i.e., the entry age is provided as the duration (in milliseconds) from the event (when entry was recorded) to the iterator initialization time.
otHistoryTrackerIterateNetInfoHistory#
const otHistoryTrackerNetworkInfo * otHistoryTrackerIterateNetInfoHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the network info history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
A pointer to
otHistoryTrackerNetworkInfoentry orNULLif no more entries in the list.
otHistoryTrackerIterateUnicastAddressHistory#
const otHistoryTrackerUnicastAddressInfo * otHistoryTrackerIterateUnicastAddressHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the unicast address history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
A pointer to
otHistoryTrackerUnicastAddressInfoentry orNULLif no more entries in the list.
otHistoryTrackerIterateMulticastAddressHistory#
const otHistoryTrackerMulticastAddressInfo * otHistoryTrackerIterateMulticastAddressHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the multicast address history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
A pointer to
otHistoryTrackerMulticastAddressInfoentry orNULLif no more entries in the list.
otHistoryTrackerIterateRxHistory#
const otHistoryTrackerMessageInfo * otHistoryTrackerIterateRxHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the RX message history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
The
otHistoryTrackerMessageInfoentry orNULLif no more entries in the list.
otHistoryTrackerIterateTxHistory#
const otHistoryTrackerMessageInfo * otHistoryTrackerIterateTxHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the TX message history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
The
otHistoryTrackerMessageInfoentry orNULLif no more entries in the list.
otHistoryTrackerIterateNeighborHistory#
const otHistoryTrackerNeighborInfo * otHistoryTrackerIterateNeighborHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the neighbor history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
The
otHistoryTrackerNeighborInfoentry orNULLif no more entries in the list.
otHistoryTrackerIterateRouterHistory#
const otHistoryTrackerRouterInfo * otHistoryTrackerIterateRouterHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the router history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
The
otHistoryTrackerRouterInfoentry orNULLif no more entries in the list.
otHistoryTrackerIterateOnMeshPrefixHistory#
const otHistoryTrackerOnMeshPrefixInfo * otHistoryTrackerIterateOnMeshPrefixHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the Network Data on mesh prefix entry history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
The
otHistoryTrackerOnMeshPrefixInfoentry orNULLif no more entries in the list.
otHistoryTrackerIterateExternalRouteHistory#
const otHistoryTrackerExternalRouteInfo * otHistoryTrackerIterateExternalRouteHistory (otInstance * aInstance, otHistoryTrackerIterator * aIterator, uint32_t * aEntryAge)
Iterates over the entries in the Network Data external route entry history list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otHistoryTrackerIterator * | [inout] | aIterator | A pointer to an iterator. MUST be initialized or the behavior is undefined. |
| uint32_t * | [out] | aEntryAge | A pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to |
Returns
The
otHistoryTrackerExternalRouteInfoentry orNULLif no more entries in the list.
otHistoryTrackerEntryAgeToString#
void otHistoryTrackerEntryAgeToString (uint32_t aEntryAge, char * aBuffer, uint16_t aSize)
Converts a given entry age to a human-readable string.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | aEntryAge | The entry age (duration in msec). |
| char * | [out] | aBuffer | A pointer to a char array to output the string (MUST NOT be NULL). |
| uint16_t | [in] | aSize | The size of |
The entry age string follows the format "<hh>:<mm>:<ss>.<mmmm>" for hours, minutes, seconds and millisecond (if shorter than one day) or "<dd> days <hh>:<mm>:<ss>.<mmmm>" (if longer than one day).
If the resulting string does not fit in aBuffer (within its aSize characters), the string will be truncated but the outputted string is always null-terminated.