RNG Cryptographic#

This module includes functions that generates cryptographic random numbers.

Functions#

otRandomCryptoFillBuffer(uint8_t *aBuffer, uint16_t aSize)

Fills a given buffer with cryptographically secure random bytes.

Function Documentation#

otRandomCryptoFillBuffer#

otError otRandomCryptoFillBuffer (uint8_t * aBuffer, uint16_t aSize)

Fills a given buffer with cryptographically secure random bytes.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]aBuffer

A pointer to a buffer to fill with the random bytes.

uint16_t[in]aSize

Size of buffer (number of bytes to fill).