Includes the statistics of SRP server responses.
Public Attributes#
uint32_t
The number of successful responses.
uint32_t
The number of server failure responses.
uint32_t
The number of format error responses.
uint32_t
The number of 'name exists' responses.
uint32_t
The number of refused responses.
uint32_t
The number of other responses.
Public Attribute Documentation#
mSuccess#
uint32_t otSrpServerResponseCounters::mSuccess
The number of successful responses.
Definition at line
130
of file include/openthread/srp_server.h
mServerFailure#
uint32_t otSrpServerResponseCounters::mServerFailure
The number of server failure responses.
Definition at line
131
of file include/openthread/srp_server.h
mFormatError#
uint32_t otSrpServerResponseCounters::mFormatError
The number of format error responses.
Definition at line
132
of file include/openthread/srp_server.h
mNameExists#
uint32_t otSrpServerResponseCounters::mNameExists
The number of 'name exists' responses.
Definition at line
133
of file include/openthread/srp_server.h
mRefused#
uint32_t otSrpServerResponseCounters::mRefused
The number of refused responses.
Definition at line
134
of file include/openthread/srp_server.h
mOther#
uint32_t otSrpServerResponseCounters::mOther
The number of other responses.
Definition at line
135
of file include/openthread/srp_server.h